Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

PowerLogic P5, P7: ATS with MV CB (alternative with MV LBS: PowerLogic T300)

Protection & Control

Schneider Electric support forum about Protection Relays, Substation Controllers & RTUs, Arc Flash Devices & Systems in Medium Voltage and Low Voltage. A place to get support on product selection, installation, commissioning and troubleshooting.
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
  • EcoStruxure Power & Grid
  • Protection & Control
  • PowerLogic P5, P7: ATS with MV CB (alternative with MV LBS: PowerLogic T300)
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Araceli_Monje
Araceli_Monje Mentor
74
JuanRayo
JuanRayo Mentor
38
Arun-kumar_PS
Arun-kumar_PS Mentor
33
View All

Recommended Forums

  • Metering & Power Quality

  • SmartConnector Forum

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Solved Go to Solution
Back to Protection & Control
Start a Topic
Solved
sesa211247_brid
sesa211247_brid Troubleshooter
Troubleshooter

Posted: ‎2024-05-03 07:29 AM . Last Modified: ‎2025-05-26 12:28 AM

1 Like
9
4412
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
‎2024-05-03 07:29 AM

PowerLogic P5, P7: ATS with MV CB (alternative with MV LBS: PowerLogic T300)

Dear Expert community 

 

is there any plan to develop an ATS (Automatic Transfert Switch)  or ABT (Automatic Bus Transfert) Application  similar to the one sold by NR PCS-9651

https://www.nrec.com/en/web/upload/2019/05/08/15572827837172kuwwm.pdf 

 

they are a lot of opportunities in the Oil and Gas segment that require a such device 

 

this could be done on the Powerlogic P5 (P5T32) or P7 platform

 

if a such product is developed it will save a lot of time, money, efforts and reduce risks .

 

Hope this will be done 

 

Attachments
Labels
  • Labels:
  • Application cases
  • IEC61850
  • PowerLogic P5
  • PowerLogic P7
  • PowerLogic T300
Tags (4)
  • Tags:
  • english
  • P5 ATS
  • P7 ATS
  • T300 ATS
Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
sesa211247_brid
sesa211247_brid Troubleshooter
Troubleshooter

Posted: ‎2024-05-10 04:35 AM

0 Likes
0
4253
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
‎2024-05-10 04:35 AM

Thank You @Jinlei_Xing 

See Answer In Context

Reply
Replies 9
Jinlei_Xing
Jinlei_Xing Leader
Leader

Posted: ‎2024-05-07 10:56 PM

1 Like
3
4319
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
‎2024-05-07 10:56 PM

It's a good idea to have dedicated device for both ATS and High Speed Transfer, such as ABB SUE3000 and Siemens 7VU68. It is possible to develop such a device based on the existing P7 platform.

 Currently we have one product Micom P84H which is for High Speed Transfer, but this product is only for Chinese marking.

 

BR,

Jinlei XING

 

 

BR,

Jinlei XING

Reply
sesa211247_brid
sesa211247_brid Troubleshooter
Troubleshooter

Posted: ‎2024-05-09 01:02 AM

0 Likes
2
4296
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
‎2024-05-09 01:02 AM

Thank You for your feedback @Jinlei_Xing 

could you share some document on the Micom P84H please (datasheet and user manual) ?

Thank you 

Reply
Jinlei_Xing
Jinlei_Xing Leader
Leader

Posted: ‎2024-05-09 01:17 AM

1 Like
1
4290
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
‎2024-05-09 01:17 AM

The related P84H slides are attached. 

 

BR,

Jinlei XING

Attachments
P84H Presentation.pptx
Reply
sesa211247_brid
sesa211247_brid Troubleshooter
Troubleshooter

Posted: ‎2024-05-10 04:35 AM

0 Likes
0
4254
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
‎2024-05-10 04:35 AM

Thank You @Jinlei_Xing 

Reply
Stefan_Scharf
Stefan_Scharf Troubleshooter
Troubleshooter

Posted: ‎2024-08-16 12:10 AM

0 Likes
0
4033
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
‎2024-08-16 12:10 AM

The ATS function is planned in a later wave for P7 as a dedicated application function block, probably with wave 4 but it can be achieved already using the Fast scheme logic (FSL) & matrix together with a sufficent number of CT/VT inputs.

Reply
DMayberry
DMayberry Explorer
Explorer

Posted: ‎2024-08-19 07:00 AM

2 Likes
2
4010
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
‎2024-08-19 07:00 AM

In the US,  Digital Power has developed these Auto Throw-Over (ATO) applications for the P5 using the imbedded IsaGraf logic engine.  These applications are being used for MV gear standard ATO systems (MM, MTM, MG, MTG) as well as the foundation for Digital Power's more complex solutions.

 

Reply
sesa211247_brid
sesa211247_brid Troubleshooter
Troubleshooter

Posted: ‎2025-02-20 12:47 PM

1 Like
0
3538
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
‎2025-02-20 12:47 PM

Hello, any update about this application?

could you share the documentation and settings files ?

Reply
TomBerry
TomBerry Troubleshooter
Troubleshooter

Posted: ‎2025-02-21 07:55 AM

1 Like
0
3507
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
‎2025-02-21 07:55 AM

The T300 HU250 module has a built-in ATS function intended for distribution network operation

With SC150 modules, this can operate switches within 300ms of voltage loss.

It is feasible to create a different configuration that communicates with protection relays instead.

Reply
jualbi.SE
jualbi.SE Explorer
Explorer

Posted: ‎2026-07-14 04:44 PM

0 Likes
0
297
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
‎2026-07-14 04:44 PM

Would you share reference project for this ATS? Could you share drawings for connections and logic or functional drawings?

Thanks 
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.