2024-10-30
06:26 AM
P3 100% logic capacity used
Good morning community,
I'm in a project how to do a load transfer and the client logic, was used 100% from inputs, 94% from Logic, and 95% from outputs (Screenshot attached).
The client is requesting documentation that approves this use with full logic and guarantees that the P3 will work properly. Do you have some documents like that?
Labels
- Labels:
-
PowerLogic P3
Replies 0