Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

MiCOM P740 - PU and CU communication Capability

Protection & Control

Schneider Electric support forum about Protection Relays, Substation Controllers & RTUs, Arc Flash Devices & Systems in Medium Voltage and Low Voltage. A place to get support on product selection, installation, commissioning and troubleshooting.
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
  • EcoStruxure Power & Grid
  • Protection & Control
  • MiCOM P740 - PU and CU communication Capability
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Araceli_Monje
Commander Araceli_Monje Commander
43
Arun-kumar_PS
Commander Arun-kumar_PS Commander
21
View All

Recommended Forums

  • Metering & Power Quality

  • SmartConnector Forum

Related Products
product field
PowerLogic
Easergy MiCOM P740

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Solved Go to Solution
Back to Protection & Control
Start a Topic
Solved
Sabhanayagan_Matheswaran
Crewman Sabhanayagan_Matheswaran Crewman
Crewman

Posted: ‎2025-05-12 11:02 AM

0 Likes
2
837
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
‎2025-05-12 11:02 AM

MiCOM P740 - PU and CU communication Capability

Hi Team,

 

We are working in a tendering opportunity, were the client requirement is to have redundant Central Unit system for Busbar protection. As a standard practice, will use PU - CU communication via single fiber optic cable from Channel-1 of P742/P743 to P741 communication slot. If I follow the standard procedure, to achieve the redundancy I need to duplicate the system, which add more cost to project and there is spare constraint as well to mount the 2 x Peripheral units in switchgears.

 

Instead of proposing the duplicated system, each P742 / P743 has 2 communication channels at the relay slots, can we use 1 channel for 1 CU (Main-1) and 2nd Channel for 2 CU (Main-2). Theoretically since the PU address is same both the CU can able to read the same data and work as a Main-1 & Main-2. Is this functionally correct, does P742 / P743 is functionally can communicate to 2 CUs simultaneously both Read & Write.

Thanks,
Sabhanayagan

  • Thumbnail of Easergy MiCOM P740
    PowerLogic
    Easergy MiCOM P740
View products (1)
Labels
  • Labels:
  • Application cases
  • MiCOM range
Tags (1)
  • Tags:
  • english
Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
HenriGRASSET
Captain HenriGRASSET Captain
Captain

Posted: ‎2025-05-15 07:13 AM . Last Modified: ‎2025-05-15 07:14 AM

0 Likes
0
778
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
‎2025-05-15 07:13 AM

Hello,

 

Even if on the communication boards there are two communication channels, it is not possible to use both at the same time and thus not possible to have redundancy.

“N-1” redundancy is to be immune to one component being faulty. Having only one Central Unit to redundant Peripheral units or Peripheral units connected to redundant Central units does not provide it.

This redundancy is often done using a P740 and a P746 (one box or three box mode) that requires much less IEDs and space and provides different types of algorithms.

 

Regards

EDISON Expert

See Answer In Context

Reply
Replies 2
Araceli_Monje
Commander Araceli_Monje Commander
Commander

Posted: ‎2025-05-15 02:45 AM

0 Likes
0
792
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
‎2025-05-15 02:45 AM

@HenriGRASSET , hi, could you please support with this question about P740?, thx.

Reply
HenriGRASSET
Captain HenriGRASSET Captain
Captain

Posted: ‎2025-05-15 07:13 AM . Last Modified: ‎2025-05-15 07:14 AM

0 Likes
0
779
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
‎2025-05-15 07:13 AM

Hello,

 

Even if on the communication boards there are two communication channels, it is not possible to use both at the same time and thus not possible to have redundancy.

“N-1” redundancy is to be immune to one component being faulty. Having only one Central Unit to redundant Peripheral units or Peripheral units connected to redundant Central units does not provide it.

This redundancy is often done using a P740 and a P746 (one box or three box mode) that requires much less IEDs and space and provides different types of algorithms.

 

Regards

EDISON Expert
Reply
Preview Exit Preview

never-displayed

You must be signed in to add attachments

never-displayed
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.