Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

FIle transfer Mode P139 BCT Tool

Protection & Control

Schneider Electric support forum about Protection Relays, Substation Controllers & RTUs, Arc Flash Devices & Systems in Medium Voltage and Low Voltage. A place to get support on product selection, installation, commissioning and troubleshooting.
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
  • EcoStruxure Power & Grid
  • Protection & Control
  • FIle transfer Mode P139 BCT Tool
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Araceli_Monje
Araceli_Monje Mentor
74
JuanRayo
JuanRayo Mentor
38
Arun-kumar_PS
Arun-kumar_PS Mentor
33
View All

Recommended Forums

  • Metering & Power Quality

  • SmartConnector Forum

Related Products
product field
PowerLogic
Easergy MiCOM P14x

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Solved Go to Solution
Back to Protection & Control
Start a Topic
Solved
omerSaeed
omerSaeed
Explorer

Posted: ‎2025-01-28 12:29 AM

0 Likes
3
1744
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
‎2025-01-28 12:29 AM

FIle transfer Mode P139 BCT Tool

Hi 

 

We made customized bay using Easergy BCT Tool in relay P139-634.  To send this file in relay, relay should be in extended(loading) mode. Then via easergy tool connection has to be established in FILE TRANSFER MODE ONLY. The issue is we are unable to connect with relay in "File transfer Mode Only". 

 

Through Easergy Help , we learned that FILE Transfer Mode is only applicable for Firmware version 650 or higher. 

 

"

Extended Platform Devices

MiCOM Px30 Extended Platform Devices (firmware starting with -650) support two types of protocols for the extraction of data, namely:

  • Standard - This uses the IEC 60870-5-103 protocol
  • Extended - This uses File Transfer Mode only on the COM port of the device. The device is switched into this mode manually at the front panel. It supports all the basic IEC-103 transmission features, but it does exclude some functions.

"

 

How can we send .bct Customized bay file in relay P139 firmware 634(which is less than 650)?

 

Support requested. 

 

 

 

  • Thumbnail of Easergy MiCOM P14x
    PowerLogic
    Easergy MiCOM P14x
View products (1)
Labels
  • Labels:
  • MiCOM range
Tags (1)
  • Tags:
  • english
Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
sesa164970_brid
sesa164970_brid Troubleshooter
Troubleshooter

Posted: ‎2025-01-28 11:31 PM

0 Likes
1
1713
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
‎2025-01-28 11:31 PM

Hi omerSaeed

Device with -634 is old one and it needs own procedure to upload the BTC.

File Transfer Mode is available since -650 firmware version, 

Please follow steps from the attached guide.

Best regards

 

See Answer In Context

Attachments
Reply
Replies 3
sesa164970_brid
sesa164970_brid Troubleshooter
Troubleshooter

Posted: ‎2025-01-28 11:31 PM

0 Likes
1
1714
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
‎2025-01-28 11:31 PM

Hi omerSaeed

Device with -634 is old one and it needs own procedure to upload the BTC.

File Transfer Mode is available since -650 firmware version, 

Please follow steps from the attached guide.

Best regards

 

Attachments
Reply
omerSaeed
omerSaeed
Explorer

Posted: ‎2025-01-29 04:35 AM

0 Likes
0
1684
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
‎2025-01-29 04:35 AM

Thank you for the support. 

I will follow the steps mentioned in the procedure and update. 

 

 

Best Regards

 

Reply
babarshahzad123
babarshahzad123
Explorer

Posted: ‎2025-06-20 12:40 AM

0 Likes
0
1363
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
‎2025-06-20 12:40 AM

Dear Both,

Please support me, if BTC can be extracted (like settings file) from existing installed/configured P139-653? Which is required to configure new P139-634. Any additional comments / support is highly appreciated.
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.