Easergy P3 [P3T32] FW V30.204-1 2nd & 5th Harmonic Block Enable

Protection & Control

Schneider Electric support forum about Protection Relays, Substation Controllers & RTUs, Arc Flash Devices & Systems in Medium Voltage and Low Voltage. A place to get support on product selection, installation, commissioning and troubleshooting.
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
  • EcoStruxure Power & Grid
  • Protection & Control
  • Easergy P3 [P3T32] FW V30.204-1 2nd & 5th Harmonic Block Enable
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Araceli_Monje
Commander Araceli_Monje Commander
43
Arun-kumar_PS
Commander Arun-kumar_PS Commander
21
View All

Recommended Forums

  • Metering & Power Quality

  • SmartConnector Forum

Related Products
product field
PowerLogic
PowerLogic P2

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Solved Go to Solution
Back to Protection & Control
Start a Topic
Solved
PaterninaEnriqu
Ensign PaterninaEnriqu Ensign
Ensign

Posted: ‎2021-06-07 06:34 PM . Last Modified: ‎2023-06-08 04:43 AM

0 Likes
1
1345
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
‎2021-06-07 06:34 PM

Easergy P3 [P3T32] FW V30.204-1 2nd & 5th Harmonic Block Enable

Hello.

I am writing to find out if anyone knows what happened with the 2nd and 5th harmonic blocking function in version FW30-204-1 and how it should be implemented in this firmware version.


Below, I attach the print-screen comparing the two firmware versions.

 

01.png

 

Fig. 1 Comparison in archive FW30.204-1 and FW30.109.

 

 I tried using functions 68F2 and 68H5 (available in both firmware versions) to block the 87T from working, but it didn't work.

 

02.png

 

Fig. 2. 68F2 and 68H5 available in firmware V30.204-1 and V30.109.

 

03.png

 

Fig. 3 Blocking matrix for function 87-1 and 87-2.


In previous firmwares this feature was embedded in the 87-1 function and it worked fine.

04.png

 

I remain attentive to any comments or suggestions.

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

  • Thumbnail of PowerLogic P2
    PowerLogic
    PowerLogic P2
View products (1)
Labels
  • Labels:
  • Application cases
  • PowerLogic P3
Tags (1)
  • Tags:
  • english
Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
Juha
Captain Juha Captain
Captain

Posted: ‎2021-06-09 12:26 AM

0 Likes
0
1333
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
‎2021-06-09 12:26 AM

Hi @PaterninaEnriqu and thanks for your question.

 

Yes, indeed Easergy P3 differentials stage dI> has changed. Removal of 5th harmonic blocking is not the only changes other are invisible.

The differential stage dI> has been improved for better handing of the primary CT saturation. This allows to re-write the CT selection guidance and allow to use smaller primary CT's. That is clear benefit.

While this was done, the 2nd harmonic restrain was improved too (available from version 30.204). The inrush blocking (2nd harmonic) is improved such that it has an addition criteria for the 2nd harmonic blocking. This additional criteria requires the power transformer to change from non-energized condition to energized condition. This is made in order to improve the inrush detection security.

When all these changes were made, the 5th harmonic blocking was removed from the dI> stage. We removed the 5th harmonic blocking as we wanted to improved it also but we faced some time constraints. The 5th harmonic blocking is still available as separate function. The separate 5th harmonic blocking can be used to block the dI> stage via the blocking matrix.

 

For more information, please do not hesitate to contact me directly by an email or teams.

 

BR

 

-juha-

 

 

See Answer In Context

Tags (1)
  • Tags:
  • english
Reply
Reply 1
Juha
Captain Juha Captain
Captain

Posted: ‎2021-06-09 12:26 AM

0 Likes
0
1334
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
‎2021-06-09 12:26 AM

Hi @PaterninaEnriqu and thanks for your question.

 

Yes, indeed Easergy P3 differentials stage dI> has changed. Removal of 5th harmonic blocking is not the only changes other are invisible.

The differential stage dI> has been improved for better handing of the primary CT saturation. This allows to re-write the CT selection guidance and allow to use smaller primary CT's. That is clear benefit.

While this was done, the 2nd harmonic restrain was improved too (available from version 30.204). The inrush blocking (2nd harmonic) is improved such that it has an addition criteria for the 2nd harmonic blocking. This additional criteria requires the power transformer to change from non-energized condition to energized condition. This is made in order to improve the inrush detection security.

When all these changes were made, the 5th harmonic blocking was removed from the dI> stage. We removed the 5th harmonic blocking as we wanted to improved it also but we faced some time constraints. The 5th harmonic blocking is still available as separate function. The separate 5th harmonic blocking can be used to block the dI> stage via the blocking matrix.

 

For more information, please do not hesitate to contact me directly by an email or teams.

 

BR

 

-juha-

 

 

Tags (1)
  • Tags:
  • english
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.