Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

CPU Saitel 866 cambiar usuario y contraseña

Protection & Control

Schneider Electric support forum about Protection Relays, Substation Controllers & RTUs, Arc Flash Devices & Systems in Medium Voltage and Low Voltage. A place to get support on product selection, installation, commissioning and troubleshooting.
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
  • EcoStruxure Power & Grid
  • Protection & Control
  • CPU Saitel 866 cambiar usuario y contraseña
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Araceli_Monje
Commander Araceli_Monje Commander
43
Arun-kumar_PS
Commander Arun-kumar_PS Commander
21
View All

Recommended Forums

  • Metering & Power Quality

  • SmartConnector Forum

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Solved Go to Solution
Back to Protection & Control
Start a Topic
Solved
CPU
CPU
Cadet

Posted: ‎2025-07-08 06:33 AM

0 Likes
1
413
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
‎2025-07-08 06:33 AM

CPU Saitel 866 cambiar usuario y contraseña

Solicitud de asistencia – Cambio de usuario y contraseña en CPU Saitel 866 con VxWorks 5.5.1

Hola [Nombre],

Estoy trabajando con una CPU Saitel 866 que utiliza VxWorks 5.5.1 y necesito cambiar el nombre de usuario y contraseña

Tags (1)
  • Tags:
  • english
Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
JuanRayo
Lt. Commander JuanRayo Lt. Commander
Lt. Commander

Posted: ‎2025-08-27 12:28 AM

0 Likes
0
320
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
‎2025-08-27 12:28 AM

Hello.

 

First of all I am switching into english for the sake of clarity of the big majority of the users of this platform so I beg you to continue our chat like this.

 

You are asking for the way to change users/passwords in a CPU Saitel 866 and there are some ways.

 

1. If you remember the IP address and have connectivity I recommend you to use Easergy Builder like this.

 

JuanRayo_0-1756278961459.png

firstly add the IP address(1), read the user configuration(2) and then edit (3) what you want to change or add (4) a new user with its privilege level. Then upload the new configuration

 

2. if you can´t use an ethernet interface you also can access through serial channel (CON) 

speed:38400

data bits:8

stop bits:1

parity:None

flow control: none

Vxworks is basically a flavour of Linux with similar commands so move to the folder /flash/ edit "userLogin.xml" and adapt it to your needs.

 

3. If you add the user "target" its access level (ALEVEL) should be 250 or higher. Do not add users like "anonymous", "ftp" or "guest" to start up a ftp session.

 

 

 

 

See Answer In Context

Reply
Reply 1
JuanRayo
Lt. Commander JuanRayo Lt. Commander
Lt. Commander

Posted: ‎2025-08-27 12:28 AM

0 Likes
0
321
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
‎2025-08-27 12:28 AM

Hello.

 

First of all I am switching into english for the sake of clarity of the big majority of the users of this platform so I beg you to continue our chat like this.

 

You are asking for the way to change users/passwords in a CPU Saitel 866 and there are some ways.

 

1. If you remember the IP address and have connectivity I recommend you to use Easergy Builder like this.

 

JuanRayo_0-1756278961459.png

firstly add the IP address(1), read the user configuration(2) and then edit (3) what you want to change or add (4) a new user with its privilege level. Then upload the new configuration

 

2. if you can´t use an ethernet interface you also can access through serial channel (CON) 

speed:38400

data bits:8

stop bits:1

parity:None

flow control: none

Vxworks is basically a flavour of Linux with similar commands so move to the folder /flash/ edit "userLogin.xml" and adapt it to your needs.

 

3. If you add the user "target" its access level (ALEVEL) should be 250 or higher. Do not add users like "anonymous", "ftp" or "guest" to start up a ftp session.

 

 

 

 

Reply
Preview Exit Preview

never-displayed

You must be signed in to add attachments

never-displayed
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.