Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84652members
353995posts

Report with Model

Power Distribution and Digital

Join experts & peers to learn, share and engage about the key trends of electrical distribution around safety, availability, efficiency and connectivity, as well as power standards & regulations. From design to implementation and operation, let’s discuss how digital and software are transforming your business and your day-to-day work.

Solved
CDickinson
Cadet
0 Likes
1
343

Report with Model

I am trying to get a feel for the percentage of load for all the UPS on my network.

I need to do this for several thousand UPS.  So doing it one at a time is NOT an option. 🙂

 

Finding the reports for 'Power (Watts)' or 'Current (Amps)' is clear enough.  BUT ....

1. The report (or the sensors) return a numerical value, not a percentage.

2. There is no column for 'percentage of load'.

3. I could get a general idea of the 'Model' was one of the available columns, but it's not (this is REALLY frustrating).

 

Any ideas on how I can figure the 'percentage of load'?


Accepted Solutions
AldebaranLopez
Ensign Ensign
Ensign

Re: Report with Model

hello,

 

The % of load in a UPS can be retrieved through a communication card (if UPS is equipped with). On the other hand if you are already retrieving load you only need nominal power from each UPS to calculate it.

 

which type of UPS do you have in your installation ?

 

 

Alejandro Aldebaran Lopez
Channel Director, Commercial & Industrial; Secure Power Division

See Answer In Context

Tags (1)
1 Reply 1
AldebaranLopez
Ensign Ensign
Ensign

Re: Report with Model

hello,

 

The % of load in a UPS can be retrieved through a communication card (if UPS is equipped with). On the other hand if you are already retrieving load you only need nominal power from each UPS to calculate it.

 

which type of UPS do you have in your installation ?

 

 

Alejandro Aldebaran Lopez
Channel Director, Commercial & Industrial; Secure Power Division
Tags (1)