Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84718members
354114posts

IEEE 519-2014 Recommended current distortion limits

Power Distribution and Digital

Join experts & peers to learn, share and engage about the key trends of electrical distribution around safety, availability, efficiency and connectivity, as well as power standards & regulations. From design to implementation and operation, let’s discuss how digital and software are transforming your business and your day-to-day work.

Farid_Kadri
Crewman
Crewman
0 Likes
0
614

IEEE 519-2014 Recommended current distortion limits

Hi there,

In IEEE 519-2014, we can see in §5.2 the recommended current distortion limits for systems nominally rated 120 V through 69 kV which depends on short circuit ration (ISC/IL), these maximum harmonics current distortion are expressed in percent of IL.

For example, for 50 < ISC/IL < 100; 3 ≤ h <11 - HD = 10% and 11≤ h < 17 - HD = 4.5% …. (HD is Harmonic Distortion).

My question is the following: are these harmonic distortion limits found based on calculations (formula) or it’s just empiric values based on experience?