Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84520members
353751posts

[IEC 61439 for LV equipment April 16th 2020 webinar] - Specifications

Power Distribution and Digital

Join experts & peers to learn, share and engage about the key trends of electrical distribution around safety, availability, efficiency and connectivity, as well as power standards & regulations. From design to implementation and operation, let’s discuss how digital and software are transforming your business and your day-to-day work.

Solved
PascalL
Lieutenant Lieutenant
Lieutenant
0 Likes
1
1178

[IEC 61439 for LV equipment April 16th 2020 webinar] - Specifications

Question from Georgios Andreadis:

 

So, we have the right to request verification tests of our specified assembly from the panel builder for every project, before site installation?


Accepted Solutions
PascalL
Lieutenant Lieutenant
Lieutenant

Re: [IEC 61439 for LV equipment April 16th 2020 webinar] - Specifications

Hello,

 

If the assembly manufacturer used a system from an original manufcaturer and respect the rules from his documentation he would not have to perform additional test.

If there are some deviation(s) based on the comparison between the certification and the assembly to deliver yes additional tests can be performed.

 

Pascal Lepretre

Sytandardization Officer - Edison Expert

See Answer In Context

1 Reply 1
PascalL
Lieutenant Lieutenant
Lieutenant

Re: [IEC 61439 for LV equipment April 16th 2020 webinar] - Specifications

Hello,

 

If the assembly manufacturer used a system from an original manufcaturer and respect the rules from his documentation he would not have to perform additional test.

If there are some deviation(s) based on the comparison between the certification and the assembly to deliver yes additional tests can be performed.

 

Pascal Lepretre

Sytandardization Officer - Edison Expert