Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84702members
354078posts

Blokset switchboard horizontal transport

Power Distribution and Digital

Join experts & peers to learn, share and engage about the key trends of electrical distribution around safety, availability, efficiency and connectivity, as well as power standards & regulations. From design to implementation and operation, let’s discuss how digital and software are transforming your business and your day-to-day work.

Solved
Esperanto
Lieutenant JG
Lieutenant JG

Blokset switchboard horizontal transport

Hello all, 

I got an issue on a Blokset switchboard delivery.

 

I would need to carry it horizontally.

 

Could you validate please I can ship it this way?

 

Best regards

Esperanto


Accepted Solutions
vijayendra_vg
Crewman
Crewman

Re: Blokset switchboard horizontal transport

Dear Esperanto,

 

Good afternoon.

 

We do not recommend transporting Blokset panel in Horizontal position.

 

The panels are intended to be used in vertical position. During the designing of the panel, care has been taken to ensure to withstand the forces which is generated because of vibration in vertical position only.

During transportation in horizontal position, the Devices, busbars and sheet metal parts may get damage because of the vibrations generated during the transportation. This will affect the performance of the switchboard.

 

So, we do not recommend transporting in Horizontal position. It should be always in Vertical position only.

 

I hope it is clear now.

 

Best Regards

Vij

See Answer In Context

2 Replies 2
vijayendra_vg
Crewman
Crewman

Re: Blokset switchboard horizontal transport

Dear Esperanto,

 

Good afternoon.

 

We do not recommend transporting Blokset panel in Horizontal position.

 

The panels are intended to be used in vertical position. During the designing of the panel, care has been taken to ensure to withstand the forces which is generated because of vibration in vertical position only.

During transportation in horizontal position, the Devices, busbars and sheet metal parts may get damage because of the vibrations generated during the transportation. This will affect the performance of the switchboard.

 

So, we do not recommend transporting in Horizontal position. It should be always in Vertical position only.

 

I hope it is clear now.

 

Best Regards

Vij

MaheshReganti
Ensign Ensign
Ensign
0 Likes
0
1444

Re: Blokset switchboard horizontal transport

When it comes to material handling like lifting, loading, unloading and installation, Blokset provides 2 options which ensures use of vertical position

1) It can be carried from forklift

2) It can be lifted by using lifting rings provided on each column or shipping sections

 

Mahesh Reganti
Product manager - Blokset, LV switchboard