Ask Me About Webinar: Data Center Assets - Modeling, Cooling, and CFD Simulation Join our 30-minute expert session on July 10, 2025 (9:00 AM & 5:00 PM CET), to explore Digital Twins, cooling simulations, and IT infrastructure modeling. Learn how to boost resiliency and plan power capacity effectively.Register now to secure your spot!
Release Notes for NetShelter™ Rack Power Distribution Units and In-Line Current Meters with NMC3 Firmware v2.5.2.5
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
You have entered an invalid email address. Please re-enter the email address.
This co-worker has already been invited to the Exchange portal. Please invite another co-worker.
Please enter email address
Send InviteCancel
Invitation Sent
Your invitation was sent.Thanks for sharing Exchange with your co-worker.
Network Management Card 3 (NMC3) Operating System and NetShelter RPDU Application
AOS: 2.5.3.2
APP: 2.5.2.5
apc_hw21_rpdu2g_2-5-2-5.nmc3
Secure NMC System (SNS) Tool for RPDU
Not applicable
Not applicable
PowerNet® SNMP Management Information Base (MIB)
4.5.6
powernet456.mib
IMPORTANT: You must have a valid Secure NMC System (SNS) subscription (SWNMC3PDU-•Y-DIGI) for PDU devices to update the firmware to version 3.0 or later. You must use the SNS tool for Rack Power Distribution Units (RPDUs) to upgrade to firmware version 3.0 or later. This is the only supported upgrade method.
New Features
New Feature
APC Operating System
None
APDU9•••, AP8•••, AP7•••B, and AP71••B Applications
The LCD displays the Alarm Status to show the details of all the alarms present in the device.
Fixed Issues
Fixed Issue
APC Operating System
Downloading the Event Log via the Web UI works as expected when the language is set to Japanese.
APDU9•••, AP8•••, AP7•••B, and AP71••B Applications
If the slave ID is unavailable, Modbus will display the error message Slave Device Failure for the register addresses.
Modbus will display a value of -1 for the Peak Temperature Capture Time if the T/TH sensor is not connected to the device.
Modbus can read values for the Outlet Layout Description even if the T/TH sensor is not connected to the device.
No Invalid Value error message appears for the TH/T sensor when the config.ini file is uploaded.
If a sensor is not connected to the device, none of the interfaces will display any parameter values.
Invalid threshold values for the Temperature and Humidity parameters are not permitted.
If an invalid value is set for the wait parameter in the cold start delay, the Immediate and Never options in the device configuration will remain inactive.
The Bank and Phrase current thresholds now support decimal values to the tenth place. This feature is available in the web UI, CLI, SNMP and the config.ini file. New OIDs have been added to accommodate this change in the SNMP interfaces.
The Range value (1-99) for Network-LED blink duration is specified on the NMC web page.
Security Update
APC Operating System
The following security vulnerabilities have been addressed in this release:
CWE-200: Exposure of Sensitive Information to an Unauthorized Actor SSH Cipher Block Chaining (CBC) cipher has been removed.
CWE-523: Unprotected Transport of Credentials. Login pages do not use adequate measures to protect the user name and password while they are in transit from the client to the server. CWE-319: Cleartext Transmission of Sensitive Information. The product transmits sensitive or security-critical data in cleartext in a communication channel that can be sniffed by unauthorized actors.
The user is now referenced as an index rather than their username, for example: NMC/KrtUvuh39YtQmHbyua297g/usercfg.htm?user=2
CWE-863: Incorrect Authorization
The Network-Only user can only perform actions in the Web UI relevant to the user access level.
CWE-20: Improper Input Validation
Incoming BACnet packet sizes are now validated.
CWE-598: Use of GET Request Method With Sensitive Query Strings. This software uses the HTTP GET method to process a request and includes sensitive information in the query string of that request.
Configuration of HSTS is now independent from HTTP or HTTPS configuration. When HSTS is enabled an STS header is added to all responses over HTTPS.
Known Issues
Known Issue
APC Operating System
None
APDU9•••, AP8•••, AP7•••B, and AP71••B Applications