Ask Me About Webinar: Data Center Assets - Modeling, Cooling, and CFD Simulation Join our 30-minute expert session on July 10, 2025 (9:00 AM & 5:00 PM CET), to explore Digital Twins, cooling simulations, and IT infrastructure modeling. Learn how to boost resiliency and plan power capacity effectively.Register now to secure your spot!
Release Notes for NetShelter™ Rack Power Distribution Units and In-Line Current Meters with NMC3 Firmware v3.0.0.5
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
You have entered an invalid email address. Please re-enter the email address.
This co-worker has already been invited to the Exchange portal. Please invite another co-worker.
Please enter email address
Send InviteCancel
Invitation Sent
Your invitation was sent.Thanks for sharing Exchange with your co-worker.
Network Management Card 3 (NMC3) Operating System and NetShelter RPDU Application
3.0.0.5
Not available for download
Secure NMC System (SNS) Tool for RPDU
3.0.0.5
snst_nmc3_rpdu2g_3-0-0-5v2.exe
PowerNet® SNMP Management Information Base (MIB)
4.5.2
powernet452.mib
Network Management Device IP Configuration Utility
4.0.5
DevIPSetup.exe
IMPORTANT:You must have a valid Secure NMC System (SNS) subscription (SWNMC3PDU-•Y-DIGI) for PDU devices to update the firmware to version 3.0 or later. You must use the SNS tool for Rack Power Distribution Units (RPDUs) to upgrade to firmware version 3.0 or later. This is the only supported upgrade method.
New Features
New Feature
APC Operating System
The NMC3 platform is now IEC-62443-4-2 certified.
Support has been added for audit logging to ensure control actions and configuration changes are recorded in the Event log.
Support has been added for remote authentication via the TACACS+ protocol.
APDU9•••, AP8•••, AP7•••B, and AP71••B Applications
None
Security Update
Password security has been updated to align with the requirements for IEC 62443-4-2.
Fixed Issues
Fixed Issue
APC Operating System
Security Update
The following security vulnerabilities has been addressed in this release:
CWE-74: Improper neutralization of special elements in output used by a downstream component (injection)
CWE-79: Improper neutralization of input during web page generation (Cross-site Scripting).
APDU9•••, AP8•••, AP7•••B, and AP71••B Applications
General improvements to the help pages of the Web User Interface (Web UI)
APDU9•••, AP8•••, AP7•••B, and AP71••B Applications
Synchronized outlet groups do not function when enabled over the network. They do function when enabled locally or when enabled through the In/Out ports.
The Reset RPDU to Defaults action also resets the system settings.
APDU9••• and AP8••• Applications
The Network Port Sharing (NPS) system does not update connected units if one of the following occurred:
The upgrade file was uploaded via SCP without the original filename.
The host device was reset to factory defaults.
APDU9••• Application
It is possible to configure a PDU without a network connection as an NPS host if that PDU has been configured with a static IP address. If one or more members of your NPS group have static IP addresses and you want to manually change the NPS host, ensure the new host has a network connection before changing the host.
When using certain tools (including the MIB Browser) as an SNMP interface to set string configurations on the device, be aware that strings starting with the “#” character may be reserved for special syntax by your interface tool. These strings will be interpreted as colon-separated decimal representations of ASCII character codes and will be stored as such by the Network Management Card. For example, setting #80:68:85 will result in the string “PDU being configured on the NMC.” If values configured in this way are not valid strings (e.g. “#1”), the OID for that value may stop responding to get and set requests. To fix this OID behavior, overwrite the invalid configuration with a valid string via any non-SNMP interface.
The Rack PDU will not warn the user when they have connected too many guest devices to the NPS group. Up to 31 guest devices can be connected to an NPS group.
It may take 30 minutes or more to apply a comprehensive config.ini file to an NPS group.
If the clearing method for an outlet alarm action is set to Auto, outlets are automatically set to the non-action state when an alarm clears, regardless of what state they were in before the alarm. For example, if the alarm action is Off, the outlets are turned on when the alarm clears. This happens even if the outlets were off before the alarm started.