Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

TM3BCEIP with M21 and M241 with M580

Modicon PAC Forum

A forum for topics related to the scope of Modicon PAC offers and ecosystem along the whole lifecycle: Modicon M580 and 340, EcoStruxure Control Expert, EcoStruxure Process Expert (Unity Pro) and more.
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
  • Industrial Automation
  • Modicon PAC Forum
  • TM3BCEIP with M21 and M241 with M580
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Trinxs1
Trinxs1 Leader
19
YONGHO-KIM
YONGHO-KIM Mentor
10
ciupol
ciupol
9
View All

Recommended Forums

  • Industry Automation and Control Forum

  • Machine and Motion Control Forum

  • Alliance Partner Program System Integrator

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Solved Go to Solution
Back to Modicon PAC Forum
Start a Topic
Solved
kelvinviroja93
kelvinviroja93
Explorer

Posted: ‎2021-09-04 01:57 AM

2 Likes
1
3720
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
Posted: ‎2021-09-04 01:57 AM

TM3BCEIP with M21 and M241 with M580

I have a TM3BCEIP, TM241CE40U, and a BMEP582040.

 

I am reading IOs from the location of M241 to M580 over EthernetIP using DTM.

(Configured TM241 as EthernetIP Adapter / Slave in M580)

 

TM241 already has the maximum modules connected and I have to expand some more modules so that I bought TM3BCEIP.

 

We have two options to read the IO from TM3BCEIP to TM241.

1)Add TM3BCEIP as Ethernet IP Adapter

2)Add TM3BCEIP as Modbus TCP Slave

 

But after adding the Bus Coupler Module to TM241 by EthernetIP or ModbusTCP we can't use TM241 as Ethernet IP Adapter.

(on EcoStructure Machine Expert 2.0 we can't add the TM3BCEIP and EthernetIP Adapter Configuration at the same timer, we can use either one of them.)

 

I need very fast data interaction between M241 and M580.

 

Question 1 - Is it possible to still use M241 as EIP Adapter after adding TM3BCEIP on it?

Question 2 - Is it Possible to directly read TM3BCEIP in M580 ? (Where is the EDS file ?)
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
Farzad_Samimi
Farzad_Samimi Contributor
Contributor

Posted: ‎2021-09-16 05:54 AM

4 Likes
0
3699
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
Posted: ‎2021-09-16 05:54 AM

Hello Kelvin,

 

it is possible to directly read TM3BCEIP in M580, see the attached document. just make sure the firmware of TM3BCEIP is the same or higher than it stated in the document. the document explained Modbus TCP and Ethernet/IP communication.

See Answer In Context

Attachments
  • Tags:
  • english
Reply

Link copied. Please paste this link to share this article on your social media post.

Reply 1
Farzad_Samimi
Farzad_Samimi Contributor
Contributor

Posted: ‎2021-09-16 05:54 AM

4 Likes
0
3700
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
Posted: ‎2021-09-16 05:54 AM

Hello Kelvin,

 

it is possible to directly read TM3BCEIP in M580, see the attached document. just make sure the firmware of TM3BCEIP is the same or higher than it stated in the document. the document explained Modbus TCP and Ethernet/IP communication.

Attachments
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.