A forum for topics related to the scope of Modicon PAC offers and ecosystem along the whole lifecycle: Modicon M580 and 340, EcoStruxure Control Expert, EcoStruxure Process Expert (Unity Pro) and more.
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
You have entered an invalid email address. Please re-enter the email address.
This co-worker has already been invited to the Exchange portal. Please invite another co-worker.
Please enter email address
Send InviteCancel
Invitation Sent
Your invitation was sent.Thanks for sharing Exchange with your co-worker.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-04-0306:33 AM
Hello Fernando,
I do not see a picture, but I suppose you only have a local Quantum IO rack, and you do not want to replace the IO?
Than it's easier to replace the CPU by the 140CRA31200 ERIO drop adapter and connect this direct to the new M580 CPU.
Please keep in mind that the M580 CPU should be type BMEP584040 minimal.
When using the 140CRA31908, you can connect a complete RIO (S908 coax) network to the 140CRP93x00, which should already be available in your system. As this is not an S908 system, but only a local rack, it makes no sense to create a S908 system.