Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

MODBUS TCP/IP WRITE FUNCTION

Modicon PAC Forum

A forum for topics related to the scope of Modicon PAC offers and ecosystem along the whole lifecycle: Modicon M580 and 340, EcoStruxure Control Expert, EcoStruxure Process Expert (Unity Pro) and more.
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
  • Industrial Automation
  • Modicon PAC Forum
  • MODBUS TCP/IP WRITE FUNCTION
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Trinxs1
Trinxs1 Leader
19
YONGHO-KIM
YONGHO-KIM Mentor
10
ciupol
ciupol
9
View All

Recommended Forums

  • Industry Automation and Control Forum

  • Machine and Motion Control Forum

  • Alliance Partner Program System Integrator

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Modicon PAC Forum
Start a Topic
Kien_2512
Kien_2512
Explorer

Posted: ‎2024-07-09 08:51 PM

0 Likes
4
1679
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
Posted: ‎2024-07-09 08:51 PM

MODBUS TCP/IP WRITE FUNCTION

 

Hi everyone,

I'm currently working on establishing a connection between an M580 2040 redundant system and a DEIF AGC controller (Modbus server) using Modbus TCP/IP. I'm utilizing the DTM browser, and the Read/Write functions are performing well. However, an issue arises when I try to change parameters directly on the AGC controller screen (locally). The root cause is that the M580 continuously writes parameters to the AGC, preventing local changes.

I want to configure the system so that it only writes to the AGC when triggered by a specific action, such as pressing a button. I've attempted to use Read_Var and Write_Var, but they didn't work as expected. Can anyone assist me in achieving this functionality?

Many thanks.

  • Tags:
  • english
Reply

Link copied. Please paste this link to share this article on your social media post.

  • All forum topics
  • Previous Topic
  • Next Topic
Replies 4
Bosswaffle
Bosswaffle
Troubleshooter

Posted: ‎2024-07-11 09:02 PM

1 Like
2
1612
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
Posted: ‎2024-07-11 09:02 PM

What behavior are you experiencing with the read and write bar functions, and what is your goal? To read continuously and write based on a trigger?

Reply

Link copied. Please paste this link to share this article on your social media post.

Kien_2512
Kien_2512
Explorer

Posted: ‎2024-07-11 10:55 PM

In response to Bosswaffle
0 Likes
1
1594
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
Posted: ‎2024-07-11 10:55 PM

After reading the documentation, I was able to read and write to the device using the read_var and write_var blocks. Currently, I have 32 Modbus TCP/IP devices similar to the one mentioned. So I want to known how many devices can an M580 2040 PLC write to simultaneously using Modbus TCP? In the case of needing to use multiple write_var blocks, what should I do to prevent them from conflicting with each other?

Reply

Link copied. Please paste this link to share this article on your social media post.

Bosswaffle
Bosswaffle
Troubleshooter

Posted: ‎2024-07-17 07:44 AM

In response to Kien_2512
1 Like
0
1520
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
Posted: ‎2024-07-17 07:44 AM

In the help file it looks like the "maximum number of requests as client per scan" on a 2040 is 32. So, in theory you can write to 32 devices simultaneously, but probably not if you're also trying to read for them too. 

 

If I were you, I would make a few groups of these FB and add a counter and trigger the groups one at a time. Wait until the activity bits in the GEST array for each member of the group is zero and then trigger the next group.

Reply

Link copied. Please paste this link to share this article on your social media post.

Kien_2512
Kien_2512
Explorer

Posted: ‎2024-07-17 08:30 PM

0 Likes
0
1498
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
Posted: ‎2024-07-17 08:30 PM

Thanks for your suggestion, It's Great!!!
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.