Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

M340 support Remote IO

Modicon PAC Forum

A forum for topics related to the scope of Modicon PAC offers and ecosystem along the whole lifecycle: Modicon M580 and 340, EcoStruxure Control Expert, EcoStruxure Process Expert (Unity Pro) and more.
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
  • Industrial Automation
  • Modicon PAC Forum
  • M340 support Remote IO
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Trinxs1
Trinxs1 Leader
19
YONGHO-KIM
YONGHO-KIM Mentor
10
ciupol
ciupol
9
View All

Recommended Forums

  • Industry Automation and Control Forum

  • Machine and Motion Control Forum

  • Alliance Partner Program System Integrator

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Modicon PAC Forum
Start a Topic
Noman
Noman
Explorer

Posted: ‎2022-09-05 11:03 PM

1 Like
2
3906
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
Posted: ‎2022-09-05 11:03 PM

M340 support Remote IO

Hi Everyone,

I have inquiry regarding remote IO. Does the M340 support Ethernet Remote IO? I checked it don't. Is there  any other method to do it kindly guide me 

 

Reply

Link copied. Please paste this link to share this article on your social media post.

  • All forum topics
  • Previous Topic
  • Next Topic
Replies 2
AlastairF
AlastairF Leader
Leader

Posted: ‎2022-09-22 01:36 PM

1 Like
0
3818
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
Posted: ‎2022-09-22 01:36 PM

No the M340 does not support eRIO.

If you want to use X80 IO remotely from M340 then you need to use the BMXPRA0100 module in place of the CRA module.

Detailed in this manual:

https://www.se.com/ww/en/download/document/EIO0000000510/?searchSource=guided

 

 

  • Tags:
  • english
Reply

Link copied. Please paste this link to share this article on your social media post.

dnordenberg1
dnordenberg1
Explorer

Posted: ‎2022-10-19 08:24 AM

0 Likes
0
3774
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
Posted: ‎2022-10-19 08:24 AM

It depends on what type of remote IO you want to use. Modbus TCP remote IO works fine. If you have a CPU with etherbet port you must use READ_VAR/WRITE_VAR function blocks to access it which can be a bit messy. If you have a BMXNOE ethernet card you can use it's built in IO scanning table to just add the IP and the registers you want to exchange in there. This is then handled by the processor in the NOE card so it can poll very fast and it offloads the main CPU from doing Modbus TCP exchange. Only drawback with the IO scanner is that it supports only reading/writing holding registers, any other types has to be done with READ_VAR/WRITE_VAR function blocks (these can be used on a NOE card to, not limited to the CPU port). There is also a ethernet card that can do Ethernet/IP but it is better to use a M580 for that which have this built in, ethernet cards are not cheep so buying a M580 CPU might even cost less than a M340 plus a ethernet card.

  • Tags:
  • english
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.