Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84601members
353872posts

M340 read MODBUS device value

Modicon PAC Forum

A forum for topics related to the scope of Modicon PAC offers and ecosystem along the whole lifecycle: Modicon M580 and 340, EcoStruxure Control Expert, EcoStruxure Process Expert (Unity Pro) and more.

Solved
Vince95
Crewman
Crewman
0 Likes
1
2169

M340 read MODBUS device value

Hi all,

 

I'm new to Schneider PLC. I had try some READ VAR tutorial but I couldn't get the data. There are few uncertainty in my mind. 

1. When I using M340 with P342020 what is the ethernet and modbus VP 5V5 r.m.c? 0.1.x

2. when I add network for ethernet it is unable to build.

3. What is the code error means for array check[2]?

 

I not sure what I miss out when configuring.

Early thanks for read and help in my problem.

 

Attachments
Tags (1)

Accepted Solutions
Farzad_Samimi
Ensign Ensign
Ensign
0
2160

Re: M340 read MODBUS device value

your syntax for ADDM is not quite right, you have to use '0.0.3{IP Address}Tcp.mbs'. make sure Data variable array size is the same as NB, see the pictures attached.

See Answer In Context

Attachments
Tags (1)
1 Reply 1
Farzad_Samimi
Ensign Ensign
Ensign
0
2161

Re: M340 read MODBUS device value

your syntax for ADDM is not quite right, you have to use '0.0.3{IP Address}Tcp.mbs'. make sure Data variable array size is the same as NB, see the pictures attached.

Attachments
Tags (1)