Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

Control Expert, How to use DNP binary input commands in PLC logic from an SEL RTAC

Modicon PAC Forum

A forum for topics related to the scope of Modicon PAC offers and ecosystem along the whole lifecycle: Modicon M580 and 340, EcoStruxure Control Expert, EcoStruxure Process Expert (Unity Pro) and more.
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
  • Industrial Automation
  • Modicon PAC Forum
  • Control Expert, How to use DNP binary input commands in PLC logic from an SEL RTAC
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Trinxs1
Trinxs1 Leader
19
YONGHO-KIM
YONGHO-KIM Mentor
10
ciupol
ciupol
9
View All

Recommended Forums

  • Industry Automation and Control Forum

  • Machine and Motion Control Forum

  • Alliance Partner Program System Integrator

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Modicon PAC Forum
Start a Topic
Owen_Woodard
Owen_Woodard Explorer
Explorer

Posted: ‎2025-08-29 07:48 AM

0 Likes
1
1852
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
Posted: ‎2025-08-29 07:48 AM

Control Expert, How to use DNP binary input commands in PLC logic from an SEL RTAC

I have configured a BMENOR2200H with a server channel for receiving DNP3 binary input commands from an SEL RTAC. 

 

Within control expert these DNP3 binary inputs from the remote client are defined as bytes within control expert. I want to be able to use the correct bit within the binary input DNP3 byte to indicate on/off from a pulsed command from the automation controller. Which bit within the byte do I use to indicate on/off status? Or which bit within the byte is going to change, and how, if the remote client sends a binary input high command (ex. TRIP bkr).

 

I currently have the DNP3 remote client byte going to a BYTE TO BOOL function block within control expert but have no way to test this expect during the installation. Is the use of the BYTE TO BOOL function block to use the DNP binary input from the remote client the correct use of this data? If not, how am I supposed to utilize the DNP3 binary input command from the remote client within the PLC logic in control expert?

 

Below is an example of how i currently have the DNP3 pulsed binary input commands from the remote client being used in the program.

 

Screenshot 2025-08-29 084619.png

 

Labels
  • Labels:
  • 02. Modicon M580 ePAC
  • 06. EcoStruxure Control Expert
  • Tags:
  • english
Reply

Link copied. Please paste this link to share this article on your social media post.

  • All forum topics
  • Previous Topic
  • Next Topic
Reply 1
Siddiqui
Siddiqui Contributor
Contributor

Posted: ‎2025-09-03 06:14 AM

0 Likes
0
1802
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
Posted: ‎2025-09-03 06:14 AM

Hi @Owen_Woodard,

 

Check my comments below:

 

The BMENOR module is configured as a DNP3 server and will receive the DNP3 Binary output commands from the DNP3 Client, which is SEL RTAC.

 

On the BMENOR server configuration, you have to choose DNP3 binary output points (BO) instead of DNP3 binary input points (BI) to receive the commands from the DNP3 Client, as mentioned below:

Siddiqui_0-1756902750538.png

 

There are three possibilities for operating CROB (Control Relay Output Block using DNP3 Binary output points:

  1. Latch ON/OFF
  2. Pulse_ON
  3. Pulse_Trip_Close.

By default, the Latch ON/OFF and Pulse_ON are selected when you declare the Binary Output DNP3 point in BMENOR configuration. For Trip functionality, you have to choose the Pulse_Trip_Close option, as shown below:

Siddiqui_1-1756902750540.png

 

Double Point Mode is selected by default for the Pulse Trip Close function in the BMENOR module, as shown below:

NOTE: The following snapshots show the DNP3 Server parameter.

Siddiqui_2-1756902750544.png

 

For the Double Point Mode, you have to declare two DNP3 Binary Output points in the BMENOR module, which are grouped for the Pulse Trip Close functionality.

 

Two DNP3 BO points are declared as shown below:

Siddiqui_3-1756902750546.png

 

Siddiqui_4-1756902750547.png

Note: Two DNP3 points are declared, with point 0 acting as a closed function and point 1 acting as a trip function. 

 

I did the test with the following setup:

  • DNP3 Client Test Harness Tool from TMW.
  • DNP3 Server BMENOR2200H Module.
  • The two DNP3 BO points are declared in the BMENOR module.
  • The Client (Test Harness) issues the Binary Output (BO) command with the following option:
    • Latch_ON
    • Latch_OFF
    • Pulse_ON
    • Pulse_Trip
    • Pulse_Close

The BO structure inside the ECE DDT is in byte format (by default, and this is fixed, and cannot be changed); we are interested in only the first bit of the byte.

It depends on the programmer how it's going to use this bit; you can also use the BYTE_TO_BOOL converter to extract this first bit. I also used BYTE_TO_BOOL for both points and mapped them into two digital points, such as Command for point 0 and Trip for point 1, as shown below.

Siddiqui_5-1756902750548.png

 

Latch_ON:

Before triggering any command from the Client side:

Siddiqui_6-1756902750548.png

 

Triggered the Latch_ON command from the Client, and it's reflected inside the ECE as shown below:

Siddiqui_7-1756902750551.png

 

 

Latch_OFF:

Siddiqui_8-1756902750553.png

 

Pulse_ON:

NOTE: The pulse duration depends on how you configured it during the point configuration.

Siddiqui_9-1756902750557.png

 

I created the trending tool inside the ECE to show you the events when the value changes from 0 to 1 and then remains at 1 for the time duration that is configured in pulse duration. Once the timer expires, it reverts 1 to 0 as shown below:

Siddiqui_10-1756902750558.png

Pulse_Close:

Siddiqui_11-1756902750562.png

 

 

Pulse_Trip:

Siddiqui_12-1756902750565.png

 

The snapshots below show the pulse for ON/Close and Trip as I issued these commands multiple times:

Siddiqui_13-1756902750567.png

 

I hope the above explanation provides a fundamental understanding and guidance on using the BMENOR module to use DNP3 BO points with Trip and Close functionality.

I suggest you read the BMENOR user manual and the DNP3 standard to get more detailed information.

 

Best Regards,

MWS
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.