Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

Channel fault or lower threshold range alarm for BMXAMI0810 analog module.

Modicon PAC Forum

A forum for topics related to the scope of Modicon PAC offers and ecosystem along the whole lifecycle: Modicon M580 and 340, EcoStruxure Control Expert, EcoStruxure Process Expert (Unity Pro) and more.
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
  • Industrial Automation
  • Modicon PAC Forum
  • Channel fault or lower threshold range alarm for BMXAMI0810 analog module.
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Trinxs1
Trinxs1 Leader
19
YONGHO-KIM
YONGHO-KIM Mentor
10
ciupol
ciupol
9
View All

Recommended Forums

  • Industry Automation and Control Forum

  • Machine and Motion Control Forum

  • Alliance Partner Program System Integrator

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Modicon PAC Forum
Start a Topic
AvinashPatil
AvinashPatil Explorer
Explorer

Posted: ‎2022-09-19 10:47 PM

1 Like
4
3723
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
Posted: ‎2022-09-19 10:47 PM

Channel fault or lower threshold range alarm for BMXAMI0810 analog module.

I have BMXAMI0810 analog module with 0-10v signal type configuration (0-10000 scaling). I want to check channel fault alarm or lower threshold range alarm for the same. As sensor is 0-10v type so when I remove the power plug from sensor end it gives 0 value to PLC. As per module data sheet, lower threshold tolerance range is -1 to -1000. when signal is -1 or less than then only will receive lower range alarm. Any other way to test the same or particular channel fault alarm. Thanks

Reply

Link copied. Please paste this link to share this article on your social media post.

  • All forum topics
  • Previous Topic
  • Next Topic
Replies 4
AlastairF
AlastairF Leader
Leader

Posted: ‎2022-09-22 01:54 PM

1 Like
2
3682
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
Posted: ‎2022-09-22 01:54 PM

You can adjust the low range threshold value up to a maximum of 0 for the 0..10V range.

If your normal working signal range is above 0 then I would just write some logic to look for values below the working range (with a time delay).

Otherwise use a 0..10V:4..20mA signal conditioner and set the module to 4..20mA. A wire break will provide an alarm.

  • Tags:
  • english
Reply

Link copied. Please paste this link to share this article on your social media post.

Robert_Willis
Robert_Willis Troubleshooter
Troubleshooter

Posted: ‎2022-09-22 02:13 PM

0 Likes
0
3679
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
Posted: ‎2022-09-22 02:13 PM

1. Which platform are you using this with Modicon M340, M580 or Quantum? 

2. Is the BMXAMI0810 configured with Topological Addressing or Device DDT? The Modicon M580 supports both Topological and Device DDT in the local racks and only Device DDT the ERIO "Ethernet Remote I/O Drops".

  • Tags:
  • english
Reply

Link copied. Please paste this link to share this article on your social media post.

andreychukvolodymyr
andreychukvolodymyr
Explorer

Posted: ‎2023-06-09 08:19 PM

In response to AlastairF
0 Likes
0
3430
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
Posted: ‎2023-06-09 08:19 PM

is it dangerous to changed polarity for channel + & - ? can it damaged the channel? output voltage from channel is 0 volts. I do not have possibility to check how channel is configurated. 

if no voltage from channel , but from sensor signal in 4-20mA.

 

 

Reply

Link copied. Please paste this link to share this article on your social media post.

andreychukvolodymyr
andreychukvolodymyr
Explorer

Posted: ‎2023-06-09 08:20 PM

In response to AlastairF
0 Likes
0
3430
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
Posted: ‎2023-06-09 08:20 PM

is it dangerous to changed polarity for channel + & - ? can it damaged the channel? output voltage from channel is 0 volts. I do not have possibility to check how channel is configurated. 

 

if no voltage from channel , but from sensor signal in 4-20mA.
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.