Ask our Experts
Didn't find what you are looking for? Ask our experts!
New Community Ranking System
Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).
A forum for topics related to the scope of Modicon PAC offers and ecosystem along the whole lifecycle: Modicon M580 and 340, EcoStruxure Control Expert, EcoStruxure Process Expert (Unity Pro) and more.
Search in
Link copied. Please paste this link to share this article on your social media post.
Posted: 2022-09-19 10:47 PM
I have BMXAMI0810 analog module with 0-10v signal type configuration (0-10000 scaling). I want to check channel fault alarm or lower threshold range alarm for the same. As sensor is 0-10v type so when I remove the power plug from sensor end it gives 0 value to PLC. As per module data sheet, lower threshold tolerance range is -1 to -1000. when signal is -1 or less than then only will receive lower range alarm. Any other way to test the same or particular channel fault alarm. Thanks
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2022-09-22 01:54 PM
You can adjust the low range threshold value up to a maximum of 0 for the 0..10V range.
If your normal working signal range is above 0 then I would just write some logic to look for values below the working range (with a time delay).
Otherwise use a 0..10V:4..20mA signal conditioner and set the module to 4..20mA. A wire break will provide an alarm.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2022-09-22 02:13 PM
1. Which platform are you using this with Modicon M340, M580 or Quantum?
2. Is the BMXAMI0810 configured with Topological Addressing or Device DDT? The Modicon M580 supports both Topological and Device DDT in the local racks and only Device DDT the ERIO "Ethernet Remote I/O Drops".
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2023-06-09 08:19 PM
is it dangerous to changed polarity for channel + & - ? can it damaged the channel? output voltage from channel is 0 volts. I do not have possibility to check how channel is configurated.
if no voltage from channel , but from sensor signal in 4-20mA.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2023-06-09 08:20 PM
is it dangerous to changed polarity for channel + & - ? can it damaged the channel? output voltage from channel is 0 volts. I do not have possibility to check how channel is configurated.
if no voltage from channel , but from sensor signal in 4-20mA.
Link copied. Please paste this link to share this article on your social media post.
You’ve reached the end of your document
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.