Share Your Feedback – Help Us Improve Search on Community! Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately. Click here to take the survey
Have ideas on how to improve Modicon? Please share and get votes from Community to influence development efforts.
Search in
The Save and Restore data (to .dtx) feature is limited to restoring data to the same project with the same CPU type. If the CPU is changed within the same family (M580 level 2 to level 4) or from quantum to M580, or memory expanded the restore data is not available.
I am suggesting the following - when the restore has an issue it should have the option to do a limited restore such that either (or both)
- all variables that exist in the save file and the new project would be restored, with a warning for those not restored
- all located memory that exist in the save file and the new project would be restored.
This would provide the following advantages
- PLC upgrades would be simplified
- Potential to create standard .dtx files to load standard setpoints to different PLCs
Additionally it would be a huge benefit to be able to Export and Import data to a spreadsheet. I suggest that while online an area of the variable table could be highlighted (or maybe an animation table) and the user given the option to export data. This would create a spreadsheet with the tagname and current value (additional useful fields would be type and initial value). And importantly control export would have a function to import data which would use the tagname and value from the spreadsheet to write to those tags with the values from the spreadsheet.
This offers the following advantages
- PLC upgrades would be simplified
- spreadsheets of setpoints could be saved, examined, and restored
Link copied. Please paste this link to share this article on your social media post.
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.