Ask our Experts
Didn't find what you are looking for? Ask our experts!
New Community Ranking System
Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).
Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
Search in
Please select a country to continue with beta search.
Link copied. Please paste this link to share this article on your social media post.
One of our clients is facing issues with downloading power monitoring data from the ION8650 meters. Is there a way to connect meter directly with laptop to download the data? I see there is an optical port in the front, can that be used to connect the meter to a laptop and download monitoring data?
Link copied. Please paste this link to share this article on your social media post.
The optical port on the front is designed for an ANSI Type 2 optical probe--I believe any model on the market will do. I recommend one with a USB port and a magnetized head.
Once the drivers are installed on your laptop at the probe is connected, it will show up as a new serial port and you will be able to connect directly to the meter using ION Setup.
Link copied. Please paste this link to share this article on your social media post.
The optical port on the front is designed for an ANSI Type 2 optical probe--I believe any model on the market will do. I recommend one with a USB port and a magnetized head.
Once the drivers are installed on your laptop at the probe is connected, it will show up as a new serial port and you will be able to connect directly to the meter using ION Setup.
You’ve reached the end of your document
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.