Ask our Experts
Didn't find what you are looking for? Ask our experts!
Share Your Feedback – Help Us Improve Search on Community! Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately. Click here to take the survey
Support forum for Machine and Motion Control solutions, including Lexium MC12 and robotics, PacDrive, Modicon PLCs and I/Os, EcoStruxure Machine Expert Twin, … - from design, implementation to troubleshooting and more, by Schneider Electric
Search in
Link copied. Please paste this link to share this article on your social media post.
Posted: 2024-12-19 01:17 PM
Hi,
I am using LXM28 with a motor (BCH2). I would like to control the speed of the motor via Modbus, just do simple steps.
I have several issues for the setup:
1/ I can modify P3-06 and P4-07 with the keypad, but they are not permanent.
When I turned off and then turn on the drive, the settings go back to 0 for those parameters.
I used those parameters to be able to force the DI1-5: SON, TQL, SPD0, SPD1, Reset Fault.
Is there a way to make those settings (P3-06 and P4-07) can be saved in eeprom?
2/ With SoMove, I can see the right values of parameters P3.06 and P4.07 only if I turn the flag Exclusive ON.
Can I set the Exclusive flag on via Modbus? (Is the same as Access Lock register?)
3/ Using SOMove, I can't manage to rotate the motor. I thought by turning on SON bit I would start, the motor,
Is there a flag that needs to be turned ON?
SON is on.
SReady is ON
SPD0=1, SPD1=0
P1.09 = 1000
There is no error.
4/ What is the Modbus register to monitor the operating state?
Thank you for you support
Best,
KB
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2025-01-20 10:14 PM
For Modbus control of LXM26/28, activate permission first by P10-32(0xB40), then enable via P2-30=1(0x33C), reset fault with P0-01=0(0x102). For jog operations: P10-25(0xB32)=1(JOG+) or P10-25=2(JOG-); P4-05(0x50A)( JOG Velocity)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2025-01-20 10:14 PM
For Modbus control of LXM26/28, activate permission first by P10-32(0xB40), then enable via P2-30=1(0x33C), reset fault with P0-01=0(0x102). For jog operations: P10-25(0xB32)=1(JOG+) or P10-25=2(JOG-); P4-05(0x50A)( JOG Velocity)
Link copied. Please paste this link to share this article on your social media post.
You’ve reached the end of your document
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.