Join our 30-minute expert session on July 10, 2025 (9:00 AM & 5:00 PM CET), to explore Digital Twins, cooling simulations, and IT infrastructure modeling. Learn how to boost resiliency and plan power capacity effectively. Register now to secure your spot!

What does the "| n" mean when viewing the properties of an OPC variable in Vista workstation?

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • What does the "| n" mean when viewing the properties of an OPC variable in Vista workstation?
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next
Contributors
  • sesa177673
    sesa177673
  • Product_Support
    Product_Support

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
0 Likes
1290 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

What does the "| n" mean when viewing the properties of an OPC variable in Vista workstation?

Picard Product_Support
‎2018-09-06 03:31 PM

Issue

  • What does the "| n" mean when viewing the properties of an OPC variable in Vista workstation?
  • Problems have been encountered with OPC variables
  • Error messages such as "The object is no longer available in the servers address space",
  • Also, canonical data type or OPC data types.

Environment

Vista 5.1.X

TAC Vista OPC client

Cause

The "|n" is a reference to the data type or canonical data type as it's called in the OPC standard. In the world of OPC, the client application can be created in on one of many diverse programming languages. To resolve potential issues all OPC data types are assigned a specific Canonical Data Type. When a client application adds an OPC Item to an OPC Group it can use the default data type for the item or it can request the item with a specific canonical data type. If the OPC tool is used then the canonical is added automatically by checking with the server. It's only if variables are added manually that this information is required.

Resolution

The method used for addressing OPC variables is Folder.Variable_Name|Data_Type

 The table below details the data types: 

Data Type

Canonical Type

Size

Data Range

Boolean

11

1 Bit

True or False

Byte

17

1 Byte

0-255

Byte Array∗

8209

1 Byte times Array Size

0-255

Short

2

2 bytes

-32768 – 32767

Short Array∗

8194

2 bytes times Array Size

-32768 – 32767

BCD

18+

2 bytes

0 - 9999

BCD Array∗

8210

2 bytes times Array Size

0 - 9999

Word

18

2 bytes

0 – 65535

Word Array∗

8210

2 bytes times Array Size

0 – 65535

Long

3

4 bytes

-2,147,483,648 to 2,147,483,647

Long Array∗

8195

4 bytes times Array Size

-2,147,483,648 to 2,147,483,647

LBCD

19+

4 bytes

0 - 99999999

LBCD Array∗

8211

4 bytes times Array Size

0 - 99999999

Dword

19

4 bytes

0 – 4,294,967,295

Dword Array∗

8211

4 bytes times Array Size

0 – 4,294,967,295

Float

4

4 bytes

-(3.40 E38 – 1.40 E-45) to (1.40 E-45 – 3.40 E38)

Float Array∗

8196

4 bytes times Array Size

-(3.40 E38 – 1.40 E-45) to (1.40 E-45 – 3.40 E38)

Double

5

8 bytes

-(1.798 E308 – 4.941 E-324) to 4.941 E-324 – 1.798 E308)

Double Array∗

8197

8 bytes times Array Size

-(1.798 E308 – 4.941 E-324) to 4.941 E-324 – 1.798 E308)

Char

16

1 Byte

All Characters supported in the standard ASCII table

String

8

1 – n Bytes

All Characters supported in the standard ASCII table

Labels (1)
Labels:
  • TAC Vista
Tags (1)
  • Find more articles tagged with:
  • 7581
Was this article helpful? Yes No
No ratings

Link copied. Please paste this link to share this article on your social media post.
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.