Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

How to set the Enterprise Server IP address

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • How to set the Enterprise Server IP address
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
0 Likes
9372 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

How to set the Enterprise Server IP address

Picard Product_Support
‎2018-09-10 12:50 PM

Last Updated: Crewman ContentModerator ‎2025-09-25 02:45 AM

Issue

How to change the IP address in the EC/ES software when it is grayed out.

Product Line

EcoStruxure Building Operation

Environment

  • Building Operation Enterprise Central (EC) and Enterprise Server (ES)
  • Building Operation WorkStation

Cause

The EC/ES IP address is grayed out in the Network Tab of the Server Properties and cannot be changed.  This setting is only used to view the IP address that the server is currently using - typically the IP of the network interface card of the PC running this.  To change this setting it must be done through the Communications TAB of the server as detailed in the resolution. 

Resolution

EcoStruxure Building Operation 2.0 and above

EBO 2.0 and above now supports multiple NIC configurations, see 2.0.1 Release Notes for details, in particular, the following note.  

  • Note: That from 2.0 the server will still listen for incoming requests on all network adapters so this setting is only used for choosing which communication settings that the server will use to communicate with child servers.

This allows other IP protocols on different networks, e.g. BACnet, Modbus, etc. to communicate with the Server. 

 

It is now possible to select which network adapter the Enterprise Central and the Enterprise Server use.  See the following WebHelp Topic Configuring Network Interface Card for an Enterprise Server or for an Enterprise Central


StruxureWare Building Operation 1.9 and below 

When the IP address of the computer changes the ES will automatically update the "IP/DNS Address" in the Properties, Network tab.

If your computer has multiple network connections, ensure that the Network Interface Card (NIC) to be used for the SmartStruxure network is set to be at the top of the list in the Adapters and Bindings.

  1. Go to the computer's Control Panel > Network Connections
  2. Select "Advanced, Advanced Settings... " from the menu.
  3. In the "Connections:" section, select the Network Connection to be used and press the up arrow to move it to the top of the list.
  • For Windows 7 / Server 2008 See the following link on how to change the order of protocol bindings: How to change the network connection priority in Windows 7
  • For Windows 8 and beyond, please refer to Adapter priority setting unavailable in Windows 10

In addition to the ES Network Properties, there is also the Communication tab in the ES that lists all of the Server IP addresses in the system.

If these need to be changed this can be done by selecting the server and clicking on the "Show/ Hide Communication settings" button circled in red below.

Labels (1)
Labels:
  • EcoStruxure Building Operation
Tags (5)
  • Find more articles tagged with:
  • 11135
  • PeterLarsen21
  • PeterLarsen22
  • RobertAndriolo20
  • RobertAndriolo21
Was this article helpful? Yes No
80% helpful (4/5)
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.