Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

Installing ITA on RHEL
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
  • EcoStruxure IT Help Center
  • EcoStruxure IT Help Center Categories
  • IT Advisor
  • ITA installation and setup
  • Installing ITA on RHEL
Options
  • My Knowledge Base Contributions
  • Subscribe
  • Bookmark
  • Invite a Friend
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • EcoStruxure IT Forum

  • APC UPS Data Center & Enterprise Solutions Forum

Previous Next

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite

EcoStruxure IT Support

Submit a support request for additional assistance with EcoStruxure IT software.

Request Support

Installing ITA on RHEL

Sort by:
Views
  • Date
  • Views
  • Likes
  • Comments
  • Helpfulness
Options
  • Subscribe
  • Bookmark
  • Invite a Friend

Installing ITA 9.1.1 and newer on Red Hat Enterprise Linux 8

Installing ITA 9.0.6 or 9.0.7 on RHEL 7? Go here Installation requirements We usually don't offer support on Red Hat installations as most of our customers who use RHEL have their own ways of installing and configuring it. Prerequisite: Before starting the ITA installation procedure, make sure that the general system requirements for on-premise installations are fulfilled in addition to these: A server running RHEL 8.0 with at least minimum install selected. IMPORTANT: Installing ITA 9.1.0 on a Red Hat system is not supported.  Access to RHEL packages by using an active RHEL subscription Disk space: /data is used for indexes and ETL configuration. Minimum size 5 GB. /data/backup is used for backups. Minimum size 50 GB. Backups should always be mounted on a remote network share. /opt/jboss-as is used for the application server. Minimum size 10 GB. /var/lib/pgsql is used for the postgres database. Minimum size 30 GB. /var/log is used for log files. Minimum size 5 GB. /tmp is temporarily used for backup file creation and/or backup file restore job. It can also be temporarily used for server/ITA upgrade. IMPORTANT: This directory must be large enough to contain unpacked backup and server upgrade file(s). Calculate the minimum size as backup file size x 4 + 3 GB. Total amount of space recommended for an installation is at least 100 GB in addition to the operating system. Changes to the system The following system changes are applied during installation of the IT Advisor software. ITA will install the listed packages* if not already installed.  *You can get a list of dependent packages for Red Hat Enterprise Linux installation through your local Schneider Electric contact.  Firewalld rules are set to ITA default locked down settings. The SNMPd configuration is replaced with a ITA configuration to provide SNMP status for the ITA services. The NTP configuration is changed to use default RHEL NTP servers. This can be changed afterwards through the server management interface (Webmin). The PostgreSQL configuration is replaced and certificates for the database get generated during install. SELinux is enabled. CTRL+ALT+DELETE reboot is disabled. Root login and UseDNS in SSH is disabled. TCP Keepalive settings are modified. Network memory settings are modified. logrotate has been configured to handle ITA and PostgreSQL logs. Loading kernel module ip_vs and ip_vs_rr. The Apache configuration is modified. The Webmin configuration is modified, disabling unused modules and changing security configuration. Enabling PostgreSQL start at boot. Maximum number of files has been increased to 100000 for JBoss (dcojboss) and root users. Installing the IT Advisor server on Red Hat Enterprise Linux Download the installation file (ITAdvisor-<version no>.iso) from a location provided by the support team. To locate the telephone number for your region, visit Contact Us. Note: The below commands should be run with root credentials. Upload the installation file to: /tmp/ Create ISO mount point /tmp/iso Mount the installer by running the command: mount -o loop /tmp/EcoStruxureITAdvisor-<version no>.iso /tmp/iso (where you replace <version no> with the 9.x.x version number) Install additional repositories containing some perl packages required by ITA: sudo yum install --assumeyes https://dl.fedoraproject.org/pub/epel/epel-release-latest-8.noarch.rpm sudo dnf config-manager --set-enabled codeready-builder-for-rhel-8-x86_64-rpms Execute the install script:  bash /tmp/iso/dco-install/install.sh Un-mount ISO: umount /tmp/iso/ Non-mandatory creation of users and groups During the installation process the setup script will automatically create these user accounts: dcojboss, dcoplat, postgres, and apache. If required, these accounts may be manually added by executing these commands with root credentials prior to installation: Add dcojboss user and group groupadd --system dcojboss useradd --system -g dcojboss --shell /bin/nologin --home-dir /opt/jboss-as -c "IT Advisor Application Server" --create-home dcojboss Add dcoplat user and group groupadd --system dcoplat useradd --system -g dcoplat --shell /bin/sh --home-dir /home/dcoplat -c "IT Advisor Platform User" --create-home dcoplat Add postgres user groupadd -g 26 -o -r postgres useradd -M -n -g postgres -o -r -d /var/lib/pgsql -s /bin/bash -c "PostgreSQL Server" -u 26 postgres  The postgres package performs the above commands. Changing UID/GID is currently untested. Add apache user groupadd -g 48 -r apache useradd -c "Apache" -u 48 -g 48 -s /sbin/nologin -r -d /usr/share/httpd apache The httpd package performs the above commands. Changing UID/GID is currently untested. Installing  IT Advisor clients Prerequisite: The server installation has been completed. On the computer where you want to install the IT Advisor client, open a web browser and launch to the IP address or hostname of the ITA server  <serverIPaddress>  to log in to the web client and get access to the desktop client download. (The ITA web client is automatically available with the server installation.) If you're not an English speaker, select your preferred language from the profile menu Language option (profile image in the upper right corner). In Administration > Licenses add your license keys to enable download according to your purchased licenses. In the profile menu select Download Desktop Clients. On the download page click to download the IT Advisor software according to your license and follow the instructions in the installation wizard. Repeat the above steps on all client computers.
View full article
Picard EcoStruxureIT
‎2020-07-31 05:58 AM

3372 Views

Installing ITA on Red Hat Enterprise Linux 7 and 8

ITA 9.1.1 and newer supports installation on RHEL 8 only. See Installing ITA 9.1.1 and newer on Red Hat Enterprise Linux 8 Installing ITA 9.1.0 on a Red Hat operating system is not supported. IT Advisor 9.0.6 has a known bug that prevents manually installing ITA on Red Hat 7.x and CentOS 7.x servers. To manually install ITA, you must use ITA 9.0.7. To install IT Advisor 9.0.6 and 9.0.7 you must use the online version of the installer ISO file, EcoStruxureITAdvisor<version>.iso. Do not use the ITA ISO file that contains the word offline - it will not work. Installation requirements We usually don't offer support on Red Hat installations as most of our customers who use RHEL have their own ways of installing and configuring it. Prerequisite: Before starting the ITA installation procedure, make sure that the general system requirements for on-premise installations are fulfilled in addition to these: A server running RHEL with at least minimum install selected. Access to RHEL packages by using an active RHEL subscription Disk space: /data is used for indexes and ETL configuration. Minimum size 5 GB. /data/backup is used for backups. Minimum size 50 GB. Backups should always be mounted on a remote network share. /opt/jboss-as is used for the application server. Minimum size 10 GB. /var/lib/pgsql is used for the postgres database. Minimum size 30 GB. /var/log is used for log files. Minimum size 5 GB. Total amount of space recommended for an installation is at least 100 GB in addition to the operating system. Optional: Due to a bug in the Red Hat Linux kernel, it is recommended to upgrade to 3.10.0-327.22.2.el7 or later. Some audit log messages may not be logged if you have a kernel version earlier than  3.10.0-327.22.2.el7 . Note: If special configuration has been done, ensure the sudoers file /etc/sudoers includes the following lines before installing or upgrading:  ## Allow root to run any commands anywhere root ALL=(ALL) ALL ## Read drop-in files from /etc/sudoers.d (the # here does not mean a comment) #includedir /etc/sudoers.d If, for security reasons, you do not want to enable one or both of the above lines, contact Technical Support for a list of changes needed for the installation to proceed. For optimum support, supply your sudoers configuration in your support request. Changes to the system The following system changes are applied during installation of the IT Advisor software. ITA will install the listed packages* if not already installed.  *You can get a list of dependent packages for Red Hat Enterprise Linux installation through your local Schneider Electric contact.  Firewalld rules are set to ITA default locked down settings. The SNMPd configuration is replaced with a ITA configuration to provide SNMP status for the ITA services. The NTP configuration is changed to use default RHEL NTP servers. This can be changed afterwards through the server management interface (Webmin). The PostgreSQL configuration is replaced and certificates for the database get generated during install. The Keepalived configuration is replaced. SELinux is enabled. CTRL+ALT+DELETE reboot is disabled. Root login and UseDNS in SSH is disabled. TCP Keepalive settings are modified. Kernel shared memory, huge pages and network memory settings are modified. logrotate has been configured to handle ITA and PostgreSQL logs. Loading kernel module ip_vs and ip_vs_rr. The Apache configuration is modified. The Webmin configuration is modified, disabling unused modules and changing security configuration. Enabling PostgreSQL start at boot. Maximum number of files has been increased to 100000 for JBoss (dcojboss) and root users.   Installing the IT Advisor server on Red Hat Enterprise Linux Download the installation file (ITAdvisor-<version no>.iso) from a location provided by the support team. To locate the telephone number for your region, visit Contact Us. Note: The below commands should be run with root credentials.   Upload the installation file to: /tmp/ Create ISO mount point /tmp/iso Mount the installer by running the command: mount -o loop /tmp/EcoStruxureITAdvisor-<version no>.iso /tmp/iso (where you replace <version no> with the 9.x.x version number) Make sure to add the optional rpms repository from your subscription link: subscription-manager repos --enable rhel-7-server-optional-rpms for RedHat 8: sudo dnf config-manager --set-enabled codeready-builder-for-rhel-8-x86_64-rpms Execute the install script:  bash /tmp/iso/dco-install/install.sh   Un-mount ISO: umount /tmp/iso/   Non-mandatory creation of users and groups During the installation process the setup script will automatically create these user accounts: dcojboss, dcoplat, postgres, and apache. If required, these accounts may be manually added by executing these commands with root credentials prior to installation: Add dcojboss user and group groupadd --system dcojboss useradd --system -g dcojboss --shell /bin/nologin --home-dir /opt/jboss-as -c "IT Advisor Application Server" --create-home dcojboss Add dcoplat user and group groupadd --system dcoplat useradd --system -g dcoplat --shell /bin/sh --home-dir /home/dcoplat -c "IT Advisor Platform User" --create-home dcoplat Add postgres user groupadd -g 26 -o -r postgres useradd -M -n -g postgres -o -r -d /var/lib/pgsql -s /bin/bash -c "PostgreSQL Server" -u 26 postgres  The postgres package performs the above commands. Changing UID/GID is currently untested. Add apache user groupadd -g 48 -r apache useradd -c "Apache" -u 48 -g 48 -s /sbin/nologin -r -d /usr/share/httpd apache The httpd package performs the above commands. Changing UID/GID is currently untested. Installing  IT Advisor clients Prerequisite: The server installation has been completed. On the computer where you want to install the IT Advisor client, open a web browser and launch to the IP address or hostname of the ITA server  <serverIPaddress>  to log in to the web client and get access to the desktop client download. (The ITA web client is automatically available with the server installation.) If you're not an English speaker, select your preferred language from the profile menu Language option (profile image in the upper right corner). In Administration > Licenses add your license keys to enable download according to your purchased licenses. In the profile menu select Download Desktop Clients. On the download page click to download the IT Advisor software according to your license and follow the instructions in the installation wizard. Repeat the above steps on all client computers.
View full article
Picard EcoStruxureIT
‎2019-10-14 08:34 AM

2496 Views
Didn't find what you are looking for? Ask our Experts
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.