Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84560members
353828posts

Installation of remote monitoring solution to older model pumping stations

Industry Automation and Control Forum

This forum is addressing industrial automation design & engineering, operations, asset performance, cyber security and digital transformation for Plants & Machines.

Solved
Ana_Martin
Administrator Administrator
Administrator
3
4087

Installation of remote monitoring solution to older model pumping stations

I’m searching for a simple way to install a remote monitoring solution to older model pumping stations, with different makes and models spanning many years and which are scattered over a large area.
Everything is running fine - until it’s not, maintenance costs are rising and frankly it’s pure luck if I catch an issue which can result in component failure.


Accepted Solutions
Omnio
Ensign
Ensign
0
4079

Re: Installation of remote monitoring solution to older model pumping stations

This is a prime example of why IoT solutions need to be cost effective and easy to deploy.

 

For this to be a relatively simple solution, you need a basic IoT monitoring setup in the cloud, affordable gateways, and most important, software that deals with the onboarding process without any additional programming being required.

 

The fact that the setup involves many groups of presumably only a few devices, in clusters spread far and wide, means you can opt for simplicity and low cost over processing power on the hardware side, although cellular capability would probably be a must. Omnio software can run on most architectures and seamlessly onboard legacy devices to any IIoT platform, making it easy to install remote monitoring systems with no retrofit needed. Measures like this will give you the safeguards you need without blowing the bank, and you can send technicians where they a needed for maintenance and repairs before critical failures.

 

More info on our onboarding plug-and-play solution:
https://shop.exchange.se.com/apps/37741/omnio-plug-play-onbording

See Answer In Context

Attachments
3 Replies 3
Omnio
Ensign
Ensign
0
4080

Re: Installation of remote monitoring solution to older model pumping stations

This is a prime example of why IoT solutions need to be cost effective and easy to deploy.

 

For this to be a relatively simple solution, you need a basic IoT monitoring setup in the cloud, affordable gateways, and most important, software that deals with the onboarding process without any additional programming being required.

 

The fact that the setup involves many groups of presumably only a few devices, in clusters spread far and wide, means you can opt for simplicity and low cost over processing power on the hardware side, although cellular capability would probably be a must. Omnio software can run on most architectures and seamlessly onboard legacy devices to any IIoT platform, making it easy to install remote monitoring systems with no retrofit needed. Measures like this will give you the safeguards you need without blowing the bank, and you can send technicians where they a needed for maintenance and repairs before critical failures.

 

More info on our onboarding plug-and-play solution:
https://shop.exchange.se.com/apps/37741/omnio-plug-play-onbording

Attachments
CdeLimerville
Ensign
Ensign
0 Likes
0
4049

Re: Installation of remote monitoring solution to older model pumping stations

Let's see on Exchange about the SE Pumping Advisor offer.

Senseye
Crewman
Crewman
0 Likes
0
4036

Re: Installation of remote monitoring solution to older model pumping stations

Hi Anna, sounds like quite a common issue and fortunately one that lots of companies are working to solve with some solid solutions. 

 

@Omnio may well be a good solution to help you to retrofit legacy assets in order to start getting data from them, when that happens, unless you have some in-house data / condition monitoring expertise then you will likely get swamped with the voluem and complexity of the data.

 

For legacy equipement, you won't want (or need) to create custom models so I would suggest you take a look at a product like Senseye which can automate the analysis of all of this data, giving you simple machine health analysis and helping you to understand which machines to focus your attention on.

 

Please check out Senseye on the Scheider Electric Exchange below or ping us an email at hello@senseye.io

https://shop.exchange.se.com/apps/34926#!overview 

Attachments