Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84521members
353757posts

IMC Example

Industry Automation and Control Forum

This forum is addressing industrial automation design & engineering, operations, asset performance, cyber security and digital transformation for Plants & Machines.

ryanAstiefes
Cadet
0 Likes
3
1327

IMC Example

I'm working on my first model controller and am running into some road blocks. First is the %Buffer% input on the IMC. I'm not clear as to what variable goes into this input. Do I need to create an array of my PV over time for this input. Also I would like to see the IMC EFB - Extruder Temperature Control Example which is online but when I try to download it I get the following error:

 

UiApp has been deprecated. Please use HtmlService instead. (line 31, file "Code", project "upexIMCEFBAPPrequest")

 

how do I go about downloading this from Chrome?

3 Replies 3
BevanWeiss
Spock
Spock
0 Likes
0
1317

Re: IMC Example

Have you read the manual?

https://download.schneider-electric.com/files?p_enDocType=User+guide&p_File_Name=33002535_K01_000_15...

 

The link that you provide does not appear to be from a Schneider website, so I don't think you'll get much support from that.

 

The buffer doesn't need for you to do anything special with it.  Just create it of a suitable size for the delay you want to compensate for, and provide the reference for it to the IMC EFB.


Lead Control Systems Engineer for Alliance Automation (VIC).
All opinions are my own and do not represent the opinions or policies of my employer, or of my cat..
BevanWeiss
Spock
Spock
0 Likes
0
1256

Re: IMC Example

@ryanAstiefes did my answer help you with your problem, if so please mark it as the solution


Lead Control Systems Engineer for Alliance Automation (VIC).
All opinions are my own and do not represent the opinions or policies of my employer, or of my cat..
john_m
Ensign
Ensign
0
1212

Re: IMC Example

A new controller ( Relaxc) will be available in a few days on shop.exchange.
Better than IMC or predictive control and of course PID. And you will not have the drawback to  manage arrays or to identify the transfer function of your your process. You plug it and control directly your process. I you test it with the free trial version give me a feedback.Thank

Tags (1)