Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84257members
353353posts

Donwload EcoStruxure™ Plant Builder 5.0 released!

Industry Automation and Control Forum

This forum is addressing industrial automation design & engineering, operations, asset performance, cyber security and digital transformation for Plants & Machines.

Rodrigo_Garcia
Administrator Administrator
Administrator
0 Likes
6
2572

Donwload EcoStruxure™ Plant Builder 5.0 released!

This release correct minors bugs mainly on the Graphical Editor found. It also introduce the CPQ export that allow to use the Bill of Material on CPQ

 

DOWNLOAD NOW

 

The EcoStruxure Plant Builder is a quotation pre-sales tool that satisfies the needs of each player in the solution selling process.

It is a standalone tool that is always in line with the latest release of EcoStruxure Plant catalog.

Starting from a project specification, the tool proposes and validates a system configuration comprising:

  • PAC modules
  • devices
  • network
  • software

It provides the complete BOM (Bill Of Material) of the full porject with pricing for project bidding, a customized system architecture drawing and a project quotation report.

 

 

Rodrigo G. 


Industrial Automation Community manager

6 Replies 6
Omaelk
Administrator Administrator
Administrator
0 Likes
0
2476

Re: Donwload EcoStruxure™ Plant Builder 5.0 released!

thanks for sharing

Tags (1)
mohammed_abdulf
Cadet
0 Likes
1
2401

Re: Donwload EcoStruxure™ Plant Builder 5.0 released!

there is no link to download . how I can download?

Tags (1)
Rodrigo_Garcia
Administrator Administrator
Administrator
0 Likes
0
2341

Re: Donwload EcoStruxure™ Plant Builder 5.0 released!

You can find the link in the post. But in any case you can use this one:

 

EcoStruxure™ Plant Builder 5.0  

 

Regards

 

Rodrigo.-

Rodrigo G. 


Industrial Automation Community manager

Tags (1)
kresekjoy
Crewman
Crewman
0 Likes
0
2279

Re: Donwload EcoStruxure™ Plant Builder 5.0 released!

Hi,
My installation stuck at the SESU update section.
Previously I have installed Version 4.5 and I have uninstalled it
What should I do?

Tags (1)
MVT
Crewman Crewman
Crewman
0 Likes
1
1570

Re: Donwload EcoStruxure™ Plant Builder 5.0 released!

Hi,

 

Thanks for Sharing!

I was able to install the software but not able to start the Control Expert configuration as it says "EcoStruxure Control Expert is not installed" where actually I have installed it. Is there a specific version of CE that it is compatible with?

 

Awaiting your support!

Tags (1)
Christophe
Ensign Ensign
Ensign
0 Likes
0
1567

Re: Donwload EcoStruxure™ Plant Builder 5.0 released!

The latest revision is EcoStruxure Architecture Builder V6 here. It supports EcoStruxure Control Expert V15.0, if you installed V15.1 you will need to wait a couple of weeks for the Builder to support V15.1

Tags (1)