Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

Converting an Modbus RTU protection relay (VIP410) to communicate measurements to client BMS by TCP using M221

Industry Automation and Control Forum

This forum is addressing industrial automation design & engineering, operations, asset performance, cyber security and digital transformation for Plants & Machines.
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
  • Industrial Automation
  • Industry Automation and Control Forum
  • Converting an Modbus RTU protection relay (VIP410) to communicate measurements to client BMS by TCP using M221
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Bastian_Schmitz
Admiral Bastian_Schmitz Admiral
35
LeTomas
Lt. Commander LeTomas Lt. Commander
14
JerryBartlemay
Lieutenant JG JerryBartlemay Lieutenant JG
7
View All

Recommended Forums

  • Machine and Motion Control Forum

  • Alliance Partner Program System Integrator

Related Products
product field
Schneider Electric
Logic Controller - Modicon M221
product field
Schneider Electric
EcoStruxure™ Machine Expert - Basic

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Industry Automation and Control Forum
Start a Topic
Yarom
Lieutenant Yarom Lieutenant
Lieutenant

Posted: ‎2024-11-11 06:32 AM

0 Likes
1
1154
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
Posted: ‎2024-11-11 06:32 AM

Converting an Modbus RTU protection relay (VIP410) to communicate measurements to client BMS by TCP using M221

Hi,

 

I am almost done with the application.

 

I have a VIP410 protection relay with Modbus RTU.  I am required to convert that and data regarding switchgear states to client BMS through Modbus TCP.

 

I have an M221. I configured the digital inputs and can read their states using Doctor Modbus (or any other Modbus application).

 

I configured on the M221 Modbus RTU IO Scanner with a set of addresses.  I have 2 VIP410 units. Device ID 1 and 2.  I am able to read on the PLC both.  However, I cannot read more than just one register. I do not know what address I am supposed to read from.

 

 

 

This works. I am able to read in Machine Expert - Basic the current values on the registers I configured.

 

My question, plain and simple, what is the address that I should be reading in Doctor Modbus? I tried 100, there is nothing. I tried 1, nothing. I set both device channel details to be the same as I am to read the same registers from each device.

 

Yarom_1-1731334579364.png

 

Here is the table I am referring to from the VIP410:

 

Yarom_2-1731334727314.png

I set the channel to start with register 1024 and took 12 length for the number of registers.

 

I did the same for the Device ID 2.

 

Here is the reading by the PLC:

 

Yarom_3-1731334886542.png

 

Here is what Doctor Modbus sees:

 

Yarom_4-1731334937221.png

 

It reads the right current that I am injecting at register 1 which is (as I assume) 100.0.0 of the PLC.

 

I can I not find the one of device 2?

 

I continued with my test on device 1 and moved the injection to phase 2 of both panels. In the PLC I am able to read the phase 2 current at 100.0.1 but I cannot see it in Doctor Modbus. I am not sure of which address to read from.

 

What am I missing?

 

Thank you for the assistance.

 

Yarom

 

 

Labels
  • Labels:
  • Process Automation Talks
  • Tags:
  • english
Reply

Link copied. Please paste this link to share this article on your social media post.

  • All forum topics
  • Previous Topic
  • Next Topic
Reply 1
Bastian_Schmitz
Admiral Bastian_Schmitz Admiral
Admiral

Posted: ‎2024-11-12 12:25 PM

1 Like
0
1118
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
Posted: ‎2024-11-12 12:25 PM

Hi,

So far I see you write all values from the IO Scanner to the same %MW. Is the one value which you get correct? Did you use FC3 or FC4 in the channel configuration? Did you check to start at 1023 or 1025?

Some Devices start at Register 0 some at Register 1.

Did you check the status of the IOScanner ?

Bastian_Schmitz_0-1731443072761.png

 

And finally you could do this easier. If you only need to convert Modbus RTU into Modbus TCP you could direct use TM172SIG. This need only be to configured via webserver as Gateway and then the BMS could directly read the RTU values via TCP.
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.