Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

EcoStruxure Geo SCADA Expert 4 | Introducing Geo SCADA 2019

Industrial Automation How-to videos

How-to videos on Schneider Electric Industrial Automation products and solutions. In general, these videos help provide a clear demonstration on the best method to accomplish a given task.
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
  • Industrial Automation How-to videos
  • EcoStruxure Geo SCADA Expert 4 | Introducing Geo SCADA 2019
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Top Labels
Top Labels
  • Alphabetical
  • Configuration and Programming 111
  • How-to & Best practices 45
  • Telemetry 42
  • Communication protocols 23
  • Solution 15
  • SCADAPack 14
  • Cybersecurity 11
  • Training & How to 9
  • Best Practice 9
  • Wireless 8
  • Realift 7
  • Integration 5
  • Licensing 4
  • How to 3
  • Asset Link 2
  • Harmony 2
  • Selection & sizing 2
  • Control Expert 2
  • Flow Computation 2
  • Smart Design & Engineering 2
  • Application Programming 2
  • Vijeo Viewer 1
  • Commissioning 1
  • Webgate 1
  • Industrial device 1
  • telepace 1
  • EcoStruxure secure connect 1
  • How-to 1
  • Utility Knowledge Base 1
  • Modicon PAC 1
  • M340 1
  • Vijeo Designer 1
  • troubleshooting 1
  • Previous
  • 1 of 4
  • Next
Latest Blog Posts
  • How to size your solar installation with Altivar Solar Sizer?
  • How to reduce harmonics with passive filter on ATV600, ATV900?
  • How to Configure Flowmeter Function on Altivar Solar ATV320?
  • How to Configure Pulse Counter Function on Altivar Solar ATV320?
  • How to use Industrial Device with EcoStruxure Secure Connect?
Related Products
product field
Schneider Electric
EcoStruxure™ Geo SCADA Expert

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Jimi
Jimi Troubleshooter
Troubleshooter
‎2020-03-23 05:54 AM
0 Likes
0
2142
  • Mark as New
  • Mark as Read
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
‎2020-03-23 05:54 AM

EcoStruxure Geo SCADA Expert 4 | Introducing Geo SCADA 2019

Originally published on Industrial Automation How-to videos by Jimi | March 23, 2020 01:54 PM

 

The 4th in this series of Geo SCADA tutorials, this video introduces our new release for Geo SCADA Expert 2019, covering exciting new features and benefits.

 
In brief, the main features are as follows:
 
- This release is the first to be named with the EcoStruxure family name: Geo SCADA will be seen on the splash screens, About boxes, F1 help, and the Installers. It will be the new name on the Resource Center, and on the new Forum in Exchange. Also for the Mobile Server.
 
A change of name, but no big changes under the hood. This will make system upgrades as simple as possible. There are no changes to registry, file locations or programming interfaces, leading to a simple install and upgrade.
 
- The flagship feature is the HTML5 Web Client called Virtual Viewx.  It can support any modern browser on PCs and tablets. We have gone back to the foundation of using ViewX for this feature, which means we have many features which WebX could not support, such as the full alarm banner with filtering, multi-Server connections, inset windows and Favorites.
 
  • Virtual ViewX supports mimics, maps, popup lists, trends and search, including script extensions to alarm banner and connects to multiple Geo SCADA Expert servers for redundant or extra databases.
  • The Browser connects to the Web server and requests login, and screen virtualization technology handles the displays. Multiple web servers can be added to share the load
  •  Licenses for WebX were previously held by the ClearSCADA servers, now they need to be purchased for the Web servers
 
- A new protocol called MQTT: An Internet of Things (IoT) protocol, designed for simpler devices.
  • MQTT protocol itself doesn’t specify a content for the data, so to kickstart our development we designed a simple format we call JSON A.
  • In the future we’ll add more protocol contents such as Sparkplug B and WITS-IoT.
  • Security is taken care of with TLS and certificates.
  • The driver is configured and works very much like other drivers, with objects representing the Broker – a kind of channel, and the Device 
  • With MQTT, a ‘cloud’ of devices is connected to a Broker – a 3rd party software process – often Open Source brokers are used. The Geo SCADA MQTT Driver connects to the broker and subscribes to data from the devices. You can see the simple data format we’re using. 
 
- Further presentation material about how Vurtual ViewX works, how to design the architecture, and the new requirements for licensing, are available.
 
 
Two additional features in this build:
 
- Alarm redirection has been extended to allow a Geo SCADA object method to be run; passing alarm redirection phone and message details.
 
- And for the convenience of Administrators, they can now access Server tools directly from ViewX.
 
 
Never miss any update by watching our full playlist of EcoStruxure Geo SCADA software videos
 
Our experts are ready to answer your questions and technical issue on Geo SCADA Expert forum and SCADA and Telemetry Devices forum 
Labels:
  • Configuration and Programming

  • Telemetry

  • Tags:
  • demo
  • ecostruxure
  • EcoStruxure Geo SCADA Expert
  • geoscada
  • SCADA integration
  • SCADA programming
  • SCADA software
  • SCADA tutorial
  • video

Author

Biography

Jimi

Link copied. Please paste this link to share this article on your social media post.

  • Back to Blog
  • Newer Article
  • Older Article

Would you like to add a comment?

All registered members have full access to the Community and can post comments and start topics.

  • Sign in / Register
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.