Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

Machine Expert HVAC - Setting a BOOL from an HMI screen

HVAC and Pumping Forum

Support Forum for HVAC and pumping machines, Modicon M17x and EcoStruxure Machine Expert HVAC software for chillers, AHU, CRAC units for datacenters or process chillers applications - from design, implementation to troubleshooting and more, by Schneider Electric.
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
  • Industrial Automation
  • HVAC and Pumping Forum
  • Machine Expert HVAC - Setting a BOOL from an HMI screen
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
FedericoM
FedericoM Mentor
119
Bastian_Schmitz
Bastian_Schmitz Champion
64
M_Cervati
M_Cervati Troubleshooter
18
View All

Recommended Forums

  • Industry Automation and Control Forum

  • Machine and Motion Control Forum

  • Alliance Partner Program System Integrator

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Solved Go to Solution
Back to HVAC and Pumping Forum
Start a Topic
Solved
RichB
RichB
Explorer

Posted: ‎2025-09-18 11:49 PM

0 Likes
4
909
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
Posted: ‎2025-09-18 11:49 PM

Machine Expert HVAC - Setting a BOOL from an HMI screen

Hello,

I have (analog) variables configured in the "Programming" tab that are accessible, displayed and modified on the screens in "Display" tab, and these all work fine.

 

I need to toggle a BOOL variable when clicking a button on a screen. The only way I see to do this is by calling a procedure via the "Events" tab. However, when compiling, an error comes up saying "Object not found" referring to the programming variable coded in the procedure.

If I declare a global BOOL variable in the HMI / Display and use that in the procedure, it works fine an I can toggle it. The problem with that is, I cannot use/find that variable in the Programming section.

 

The reason I'm trying to do it via a procedure, is because the option to insert a check box on the screen is greyed-out (not sure why as the documentation states it's possible), which I'm sure would be the correct way to toggle a bit.

 

I'm developing on a M172PDG42R and the ME HAVAC version is 1.7.0.

 

Please Help...

Richard

Labels
  • Labels:
  • HVAC
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
ismailozinan
ismailozinan Leader
Leader

Posted: ‎2025-09-20 09:46 AM

0 Likes
1
887
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
Posted: ‎2025-09-20 09:46 AM

If you wish, you can also use the physical buttons on the display as toggles.
For example, in the program linked below, the physical Left button next to the display is configured as a toggle.

Click here 
You can also find a video in the program folder showing how it works.
I hope you find it helpful.

See Answer In Context

Reply

Link copied. Please paste this link to share this article on your social media post.

Replies 4
ismailozinan
ismailozinan Leader
Leader

Posted: ‎2025-09-20 05:25 AM

0 Likes
0
895
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
Posted: ‎2025-09-20 05:25 AM

You can download the sample program from this link 
Additionally, the link includes a video that you may follow if you would like to see the steps I took.

Reply

Link copied. Please paste this link to share this article on your social media post.

ismailozinan
ismailozinan Leader
Leader

Posted: ‎2025-09-20 09:46 AM

0 Likes
1
888
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
Posted: ‎2025-09-20 09:46 AM

If you wish, you can also use the physical buttons on the display as toggles.
For example, in the program linked below, the physical Left button next to the display is configured as a toggle.

Click here 
You can also find a video in the program folder showing how it works.
I hope you find it helpful.

Reply

Link copied. Please paste this link to share this article on your social media post.

obscuresc
obscuresc
Troubleshooter

Posted: ‎2025-09-21 06:23 PM

0 Likes
0
837
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
Posted: ‎2025-09-21 06:23 PM

Hi Richard,

 

Code running on the HMI (developed in the Display tab) is almost independent from the code on the PLC backend (Programming tab), which is why the Programming code cannot find the your variables in the procedures you mentioned.

 

The linkage between the two codes is via a communication layer though I am not sure what, but they exchange data though registers defined by you in Commissioning, or shared registers defined by Schneider/Eliwell/Axel. You can link a variable field to a register, basically the way @ismailozinan suggested, though this isn't really event based as you mentioned.

 

The other option is to use the 'Video_SetParam'/'Video_GetParam' functions available in the HMI editor, to initiate read/write of registers on command. These functions can take a hardcoded address to the register, or you can you the 'PAR_ADR' function which returns the register address based on the name of the register.

 

Thanks.

 

 

Reply

Link copied. Please paste this link to share this article on your social media post.

RichB
RichB
Explorer

Posted: ‎2025-09-21 09:03 PM

In response to ismailozinan
1 Like
0
802
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
Posted: ‎2025-09-21 09:03 PM

Hello Ismailozinan,

 

Thank you very much for your code and videos - they really helped. 

I implemented your second solution and I have it working as intended - toggling of eight BOOLs from the HMI screen.

 

Best Regards

Richard
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.