Ask our Experts
Didn't find what you are looking for? Ask our experts!
New Community Ranking System
Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).
Support Forum for HVAC and pumping machines, Modicon M17x and EcoStruxure Machine Expert HVAC software for chillers, AHU, CRAC units for datacenters or process chillers applications - from design, implementation to troubleshooting and more, by Schneider Electric.
Search in
Please select a country to continue with beta search.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2024-02-01 07:25 PM
Hi,
I am setting up BACnet on TM172PDG18R. I have created a device object with the following properties

After downloading the project, and connecting via Yabe, the device appears correctly.
If I attempt to change the Object Name of the Device Object, I receive an 'ERROR_CODE_WRITE_ACCESS_DENIED'.

Document EIO0000004776 06/2022 'BACnet Application Notes' indicates that this property is writable.
If I go into the Configuration pane of ESME HVAC, I can edit the register associated, and the object name in Yabe will change.
Does mean that the object name is only available for edit via Modbus or via programming on the IEC-side?
Thanks,
Jack
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2024-02-05 01:03 AM
Hello,
string properties of BACnet objects can be modified from IEC code or via Modbus in case they are published also through this protocol, they can't be modified from BACnet BMS.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2024-02-05 01:03 AM
Hello,
string properties of BACnet objects can be modified from IEC code or via Modbus in case they are published also through this protocol, they can't be modified from BACnet BMS.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2024-02-07 11:31 PM
BACnet requires UTF-8 chars while M172 and IEC code supports ASCII from Programming, so the only way to be compliant with BTL is to have read only strings from BACnet side
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
You’ve reached the end of your document
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.