modbus serial communication to P342020

Gateways and Energy Servers

Schneider Electric support forum to share knowledge about product selection, installation and troubleshooting for EcoStruxure Panel Server, PowerTag, Com'X, Link150…
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
  • EcoStruxure Power & Grid
  • Gateways and Energy Servers
  • modbus serial communication to P342020
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Romain_Polette
Kirk Romain_Polette Kirk
117
Guillaume_Evrard
Captain Guillaume_Evrard Captain
58
Randi_Dolan
Commander Randi_Dolan Commander
46
View All

Recommended Forums

  • Metering & Power Quality

  • SmartConnector Forum

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Gateways and Energy Servers
Start a Topic
shabeenek
Crewman shabeenek
Crewman

Posted: ‎2024-08-12 11:25 PM

0 Likes
2
744
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
‎2024-08-12 11:25 PM

modbus serial communication to P342020

Good day friends,

 

Im trying to receive modbus data from a power meter METSEPM5110 to controller P342020 which has serial modbus rj45 port. The meter has D1, D0, C and Shield terminals. 

On the controller side (P342020) RJ45 port, I identified 4 and 5 pins are D1 and D0 respectively and pin 8 is Common. I connected accordingly using a terminal block. 

Using the READ_VAR, I am not receiving data from meter. 

baud rate is set to 9600, parity even

Reply
  • All forum topics
  • Previous Topic
  • Next Topic
Replies 2
Bosswaffle
Lt. Commander Bosswaffle
Lt. Commander

Posted: ‎2024-08-14 06:43 AM

0 Likes
0
710
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
‎2024-08-14 06:43 AM

In Control Expert, did you setup the M340's serial port as a 2 wire RS485 modbus master running at 9600 baud with even parity? Did you change the default speed of the METSEPM5110 from 19200 to 9600? 

 

If those are both setup then:

  1. Try swapping D1 and D0.
  2. Try using the serial port on your computer or a USB to serial converter. (via modscan/kepware/topserver/etc.)
  3. Post your code here so we can review it.
Reply
shabeenek
Crewman shabeenek
Crewman

Posted: ‎2024-08-18 10:18 AM

1 Like
0
686
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
‎2024-08-18 10:18 AM

Solved brother. There was 1 offset in the modbus register. When I gave register number one less than in register in read var, data was read.

Thankyou
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.