Ask our Experts
Didn't find what you are looking for? Ask our experts!
Share Your Feedback – Help Us Improve Search on Community! Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately. Click here to take the survey
Schneider Electric support forum to share knowledge about product selection, installation and troubleshooting for EcoStruxure Panel Server, PowerTag, Com'X, Link150…
Search in
Link copied. Please paste this link to share this article on your social media post.
Hi,
is it possible to use GPRS module and wi-fi module together on a comX510 or a Comx 210 ( they should be functioning simultaneously)??
Can we send SMS alerts using ComX510?
Posted: 2015-09-18 02:26 PM
Link copied. Please paste this link to share this article on your social media post.
Guarang,
GPRS and Wifi will not work simultaneously on the ComX. There is a picture below of the network settings page showing the two are mutually exclusive. Could you describe the use case that would require these two running at the same time?
Also, the ComX doesn't currently send SMS alerts. @Joelle Key might be able to answer where that functionality fits in the roadmap.

Posted: 2015-09-23 07:44 AM
Link copied. Please paste this link to share this article on your social media post.
Guareng,
While my other answer is true, it only applies to which system you can publish through. If you are asking about using WiFi to commission a system or just connect to the web pages, you can do that. If you plug the WiFi dongle into the ComX, you will be able to connect to a WiFi network that is named the same name as the ComX, regardless of whether you have a GPRS modem installed.
Once you've connected to the WiFi network, use the address 10.25.2.1 in your browser to visit the ComX web pages.
Hope this helps.
You’ve reached the end of your document
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.