Panel Server's recommended number of TCP devices

Gateways and Energy Servers

Schneider Electric support forum to share knowledge about product selection, installation and troubleshooting for EcoStruxure Panel Server, PowerTag, Com'X, Link150…
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
  • EcoStruxure Power & Grid
  • Gateways and Energy Servers
  • Panel Server's recommended number of TCP devices
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Romain_Polette
Kirk Romain_Polette Kirk
116
Guillaume_Evrard
Captain Guillaume_Evrard Captain
58
Randi_Dolan
Commander Randi_Dolan Commander
46
View All

Recommended Forums

  • Metering & Power Quality

  • SmartConnector Forum

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Solved Go to Solution
Back to Gateways and Energy Servers
Start a Topic
Solved
Song-hee
Ensign Song-hee Ensign
Ensign

Posted: ‎2023-11-08 06:49 PM . Last Modified: ‎2023-11-08 06:53 PM

0 Likes
3
1870
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
‎2023-11-08 06:49 PM

Panel Server's recommended number of TCP devices

Hello,

We are on design and estimation stage for PAS with multiple meters, there is any recommended number of devices to the communicaion performance?

In the user guide tells 64 for max connetion, and the release notes tells 32 devices for the maximum number of Modbus/TCP concurrent connections.

I'd to avoid some trouble issue of communication performance, let me know the general connection number of slave devices with PAS.

Songhee_1-1699498398633.png

 

Songhee_0-1699498371443.png

 

Labels
  • Labels:
  • Legacy Gateways & Energy Servers
  • Product selection
Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
MarianTodorov
Ensign MarianTodorov Ensign
Ensign

Posted: ‎2023-11-09 03:47 AM

1 Like
0
1841
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
‎2023-11-09 03:47 AM

Hello,

 

My understanding on this topic is that PAS can read up to 64 devices via Modbus TCP. The 32 Modbus TCP concurrent connections are to define the limit of devices/systems which can read through PAS at the same time. For instance PME, EPO, EBO, ION devices reading data from serial devices under PAS.

 

Best regards,

Marian

See Answer In Context

Reply
Replies 3
Grant_IPACS
Commander Grant_IPACS
Commander

Posted: ‎2023-11-08 09:30 PM

1 Like
0
1859
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
‎2023-11-08 09:30 PM

64 is because you can  have a 'slave' PAS off a master PAS, both having 32 devices each maximum = 64 devices, voila!

Regards

Grant
Reply
Guillaume_Evrard
Captain Guillaume_Evrard Captain
Captain

Posted: ‎2023-11-08 09:59 PM

2 Likes
0
1857
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
‎2023-11-08 09:59 PM

Hello,

you have the modbus client that allows to connect modbus device. Limit is now 128 (1.7) instead of 64. this is the theoritical calculation but I would expect that performance testing has been made depending on the type of modbus tcp devices. I saw a calculator for EEH.

Regarding modbus server, it is a feature that allow you to poll from a modbus client data from the PAS. If you have activated modbus server on ETH1 as an example you can poll whatever device from the PAS using the Virtual id. Having maximum 64 concurrent tcp connection should be enough.

Kind Regards,

Reply
MarianTodorov
Ensign MarianTodorov Ensign
Ensign

Posted: ‎2023-11-09 03:47 AM

1 Like
0
1842
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
‎2023-11-09 03:47 AM

Hello,

 

My understanding on this topic is that PAS can read up to 64 devices via Modbus TCP. The 32 Modbus TCP concurrent connections are to define the limit of devices/systems which can read through PAS at the same time. For instance PME, EPO, EBO, ION devices reading data from serial devices under PAS.

 

Best regards,

Marian
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.