Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

Panel Server 2 DI

Gateways and Energy Servers

Schneider Electric support forum to share knowledge about product selection, installation and troubleshooting for EcoStruxure Panel Server, PowerTag, Com'X, Link150…
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
  • EcoStruxure Power & Grid
  • Gateways and Energy Servers
  • Panel Server 2 DI
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Romain_Polette
Kirk Romain_Polette Kirk
117
Guillaume_Evrard
Captain Guillaume_Evrard Captain
59
Randi_Dolan
Commander Randi_Dolan Commander
46
View All

Recommended Forums

  • Metering & Power Quality

  • SmartConnector Forum

Related Products
product field
Schneider Electric
EcoStruxure Panel Server Universal
product field
Schneider Electric
EcoStruxure Panel Server Advanced

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Solved Go to Solution
Back to Gateways and Energy Servers
Start a Topic
Solved
AndersDahlskog
Lieutenant AndersDahlskog Lieutenant
Lieutenant

Posted: ‎2023-02-17 01:03 AM

0 Likes
1
1246
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
‎2023-02-17 01:03 AM

Panel Server 2 DI

Hi

The two DI in PAS600L, PAS800L are they active or passive (Power Supply) ?, can it be configured. So the right type of pulse counter is to be used.

Is the old SIM10M unit (Modbus slave) compatible ? or planned in future firmware release

 

BR/Anders

  • Thumbnail of EcoStruxure Panel Server Advanced
    Schneider Electric
    EcoStruxure Panel Server Advanced
  • Thumbnail of EcoStruxure Panel Server Universal
    Schneider Electric
    EcoStruxure Panel Server Universal
View products (2)
Labels
  • Labels:
  • Commissioning
  • Product selection
Tags (1)
  • Tags:
  • english
Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
Thierry_Baudard
Commander Thierry_Baudard Commander
Commander

Posted: ‎2023-03-03 12:03 AM

2 Likes
0
1215
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
‎2023-03-03 12:03 AM

 

Hello

 

The two Dis of the PAS600L/PAS800L are passive. So an external power supply (24 VDC recommended if supported by the pulse counter) must be added to fix the potentials.

Electrical pulse counters compliant to standard IEC62053-31 (example iEM2000T ) can be connected to the PAS DIs.

Based on the analysis of this standard, the maximum pulse frequency should be 16.66 Hz (with a minimum pulse width of 30 ms). 

it is possible to connect wage meters (gas, water, etc...) compatible to the characteritics abover even if they are not certified IEC62053-31.

 

Regarding SIM10M:

- if the Panel Server acts as a transparent gateway, no template is needed and in this case SIM10M can be connected (like any other modbus SL product : SE or third party)

- if the panel server acts as data aggregator  (Local Energy server or cloud connection architectures), there is no Built-in model for SIM10M  in Panel Server and  you will have to develop a custom model.

 

Note: For reasons of memory size, it is not possible to embed built-in models for all SE products. The strategy is therefore to not include end-of-commercialization products (such as the SIM10M) which can be replaced by available equivalent products (such as the SmartLink A9XMSB11).

 

BR


 

 

Thierry BAUDARD
EcoStruxure Power- Technical Support Expert for Softwares & Solutions

See Answer In Context

Reply
Reply 1
Thierry_Baudard
Commander Thierry_Baudard Commander
Commander

Posted: ‎2023-03-03 12:03 AM

2 Likes
0
1216
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
‎2023-03-03 12:03 AM

 

Hello

 

The two Dis of the PAS600L/PAS800L are passive. So an external power supply (24 VDC recommended if supported by the pulse counter) must be added to fix the potentials.

Electrical pulse counters compliant to standard IEC62053-31 (example iEM2000T ) can be connected to the PAS DIs.

Based on the analysis of this standard, the maximum pulse frequency should be 16.66 Hz (with a minimum pulse width of 30 ms). 

it is possible to connect wage meters (gas, water, etc...) compatible to the characteritics abover even if they are not certified IEC62053-31.

 

Regarding SIM10M:

- if the Panel Server acts as a transparent gateway, no template is needed and in this case SIM10M can be connected (like any other modbus SL product : SE or third party)

- if the panel server acts as data aggregator  (Local Energy server or cloud connection architectures), there is no Built-in model for SIM10M  in Panel Server and  you will have to develop a custom model.

 

Note: For reasons of memory size, it is not possible to embed built-in models for all SE products. The strategy is therefore to not include end-of-commercialization products (such as the SIM10M) which can be replaced by available equivalent products (such as the SmartLink A9XMSB11).

 

BR


 

 

Thierry BAUDARD
EcoStruxure Power- Technical Support Expert for Softwares & Solutions
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.