Modbus registers from Analog and Digital input on the comX210 and comX510

Gateways and Energy Servers

Schneider Electric support forum to share knowledge about product selection, installation and troubleshooting for EcoStruxure Panel Server, PowerTag, Com'X, Link150…
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
  • EcoStruxure Power & Grid
  • Gateways and Energy Servers
  • Modbus registers from Analog and Digital input on the comX210 and comX510
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Romain_Polette
Kirk Romain_Polette Kirk
116
Guillaume_Evrard
Captain Guillaume_Evrard Captain
58
Randi_Dolan
Commander Randi_Dolan Commander
46
View All

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Solved Go to Solution
Back to Gateways and Energy Servers
Start a Topic
Solved
Mauricio_G
Crewman Mauricio_G Crewman
Crewman

Posted: ‎2015-11-06 12:37 PM

0 Likes
1
865
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
‎2015-11-06 12:37 PM

Modbus registers from Analog and Digital input on the comX210 and comX510

Hi everyone,

I have a couple customers requesting a nice and smooth WAGES solution for PME, so the question is simple, the analog and digital inputs on the ComX210 and 510 are available through Modbus registers? is there any firmware able to do it?

If someone can help me with this will be awesome

Thanks

Mauricio

Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
Anonymous user
Not applicable

Posted: ‎2015-11-16 12:37 AM . Last Modified: ‎2022-10-18 10:45 PM

1 Like
0
753
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
‎2015-11-16 12:37 AM

Hello Mauricio Alexandro

Analog Input area available on the Com'X since version 1.3.5 (Com'X 200), and since the first version of he Com'X 510.

The modbus gateway setting must be set to "Yes"

I have posted a small tutorial on the Com'X Analog Input here :

https://community.se.com/thread/20218

For Digital Input, you can also see this link :

https://community.se.com/message/68474#68474

As a summary :

If AI-1 is used, its value (coded as Float32) is available at registers 10000 and 10001 (Most significant register first)

If AI-2 is used, its value (coded as Float32) is available at registers 10002 and 10003 (Most significant register first)

If the device type is a built-in model (PT100 or PT1000), the value returned by the Modbus-TCP server is the temperature value

If the device type is a custom model (0-10V or 4-20mA), the value returned by the Modbus-TCP server is the raw value : voltage or current value

     Regards

     Jef

See Answer In Context

Reply
Reply 1
Anonymous user
Not applicable

Posted: ‎2015-11-16 12:37 AM . Last Modified: ‎2022-10-18 10:45 PM

1 Like
0
754
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
‎2015-11-16 12:37 AM

Hello Mauricio Alexandro

Analog Input area available on the Com'X since version 1.3.5 (Com'X 200), and since the first version of he Com'X 510.

The modbus gateway setting must be set to "Yes"

I have posted a small tutorial on the Com'X Analog Input here :

https://community.se.com/thread/20218

For Digital Input, you can also see this link :

https://community.se.com/message/68474#68474

As a summary :

If AI-1 is used, its value (coded as Float32) is available at registers 10000 and 10001 (Most significant register first)

If AI-2 is used, its value (coded as Float32) is available at registers 10002 and 10003 (Most significant register first)

If the device type is a built-in model (PT100 or PT1000), the value returned by the Modbus-TCP server is the temperature value

If the device type is a custom model (0-10V or 4-20mA), the value returned by the Modbus-TCP server is the raw value : voltage or current value

     Regards

     Jef
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.