Gateways and Energy Servers
Schneider Electric support forum to share knowledge about product selection, installation and troubleshooting for EcoStruxure Panel Server, PowerTag, Com'X, Link150…
User | Count |
---|---|
82 | |
46 | |
29 | |
28 |
Link copied. Please paste this link to share this article on your social media post.
Just released!!!
Downloads EGX300 Firmware & Disk Image Update Version 4.300 firmware provides: · Improved Custom Device Type Generator support – added offset · Resolution to Daylight Savings Time not operating correctly in the Southern Hemisphere · HTTP Proxy Support for Data Export · Resolution to issue exporting via SSL to IIS Web Server · Disk Image Version is displayed in the Web Interface Version 4.300 Disk Update provides: · Ability to save Dashboard images · Russian and Japanese Language support · Support for the following devices. o EM7320 o EM7380 o PM5350BW *Upgrading to version 4.300 requires new firmware to be downloaded to the EGX followed by the egx04300.upd Disk Image. |
Firmware Download Instructions for EGX300 Currently Running Firmware Version 3.7xx Updating to version 4.300 from version 3.7xx requires all data log files to be converted internally. This conversion will be executed at the first boot after the download. While converting the data log files, browsing of the EGX will be limited to a page displaying the status of the conversion until conversion is complete. Depending on the size and number of the data log files this process may take several minutes. Before downloading the firmware logging must be disabled. It is recommended the user save all data log files to external storage before downloading. Refer to the EGX300 User’s Guide for instructions on how to disable logging and remove data log files. 1. Disable Logging. 2. Save data log files to external storage (optional but recommended). 3. Remove data log files (optional but recommended). 4. Transfer the version 4.300 firmware file (egx04300.bin) to your computer. 5. Use FTP to copy the “egx04300.bin” file from your computer to the EGX300. The status LED will flash rapidly while the firmware is being programmed. Do not remove power during this time. Once the download is complete the EGX will automatically reboot. Refer to the EGX300 User’s Guide if you need more information. 6. Allow the EGX to reboot after the firmware file transfer, then browse the EGX300 Diagnostic Statistics page and confirm V4.300 is displayed as the Firmware Version in the Gateway Information section. 7. After confirming the firmware has been updated apply the V4.300 Disk Update. |
Firmware Download Instructions for EGX300 Currently Running Firmware Version 3.800 or Greater Before downloading the v4.300 firmware it is recommended to disable logging and to save all data log files to external storage. Refer to the EGX300 User’s Guide for instructions on how to disable logging and remove data log files. 1. Disable Logging. 2. Save data log files to external storage (optional but recommended). 3. Remove data log files (optional but recommended). 4. Transfer the version 4.300 firmware file (egx04300.bin) to your computer. 5. Use FTP to copy the “egx04300.bin” file from your computer to the EGX. The status LED will flash rapidly while the firmware is being programmed. Do not remove power during this time. Once the download is complete the EGX will automatically reboot. Refer to the EGX300 User’s Guide if you need more information. 6. Allow the EGX to reboot after the firmware file transfer then browse the EGX300 Diagnostic Statistics page and confirm 4.300 is displayed as the Firmware Version in the Gateway Information section. 7. After confirming the firmware has been updated apply the V4.300 Disk Update. |
Link copied. Please paste this link to share this article on your social media post.
Hi James, I tried updating two of my EGX300 currently. With both of them Firmware upgrade (.bin) file worked well, however, while putting a update patch (.upd) file, it gave me below error "An error occurred copying a file to the FTP Server. Make sure you have permissionto put files on the server. Details: The Connection with the server was reset."
With the first one after several attempts, it was resolved and was able to update the patch. Not with the second one.
Link copied. Please paste this link to share this article on your social media post.
Hello Hastak.
How long did you wait before trying to apply the v4.300.upd disk update? Perhaps this is the issue?? Once you copy the EGX300 firmware to the box via FTP...it needs to reboot the box. You must wait for it to come back online before applying the patch in the same maner...once again, a reboot I updated the EGX300 Demo Site this afternoon, and did not have any issues, but let me know what you find.
What do you see on the bottom left hand side of your EGX300? Which Disk Image Version shows?
Thanks,
James
Link copied. Please paste this link to share this article on your social media post.
Hi James, Yes I did wait till it reboots. However since then I have been able to figure out the way and I have update 2 more EGXs since then.
What I did initially was copy both bin file and upd file in System folder, one after the other. But what I did now was copied the bin file in System folder and dropped the upd file in main ftp folder on EGX. And it works perfect!
Link copied. Please paste this link to share this article on your social media post.
Perfect...let me know if you have any additional feedback about the 4.3 release. Thanks!
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.