Posted: 2015-04-02 02:08 AM
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
EGX100 Connexion lost
Hi,
Is anyone know why I lost the connection with two PM800 meter connected in the same EGX100 and after a few hours it return ?
Best regards.
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
Please check if PoE is powered on, while the power supply for the EGX is connected in parallel. If so, just disconnect the power supply of the EGX.
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
Except check PoE power supply, please check:
1) Was terminal resistance (120 ohm) connected correctly?
2) RS-485 shield ground should be one side connection instead of loop ground. It should be connected on one side, not connected on both sides.
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
Hi Amine,
Please check the answers from Alexander and Jun and assess if those are describing your PM800 connections situation or if they help.
Regards,
Adrian

Posted: 2015-04-07 08:58 AM
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
Hi Adrian,
I haven't check those answers in site but if i solve this probleme i will contact you.
Best regards.

Posted: 2015-04-07 08:58 AM
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
Thank you very uch for your help.
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
You are welcome to contact us if you require further assistance.