Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84694members
354073posts

ComX 200 - Modbus gateway support and PME7.2 support

Gateways and Energy Servers

Get expert answers to your questions regarding Schneider Electric Gateways & Energy Servers, from product selection to implementation and troubleshooting. Collaborate with a global community of experts and peers, get support and share your experiences by subscribing to the Schneider Electric Community Gateways and Energy Servers forum today.

Solved
sesa8515
Schneider Alumni (Retired)
Schneider Alumni (Retired)

ComX 200 - Modbus gateway support and PME7.2 support

Hello,

I am preparing quotation for customer where I would like to use many ComX200 + PME7.2. To finish this offer I need clarify some questions:

1. When will be released FW for CommX 200 with Modbus Gateway functionality?

2. How we can read online data from ComX digital/analog inputs from PME7.2? (Doeas ComX support Modbus slave functionality?)

3. Will PME7.2 have driver/tool for ComX 200 that will allow to synchronize data from ComX memory and PME database?

Thank you

Jan Mikulec

Tags (1)

Accepted Solutions
sesa41698_bridg
Lt. Commander Lt. Commander
Lt. Commander

Re: ComX 200 - Modbus gateway support and PME7.2 support

The modbus gateway feature will be included in Com'X 200 version 1.1

This version 1.1 will be available mid March 2014

In this version 1.1, it will not be possible to read the Digital Input neither the Analog Input in the Com'X 200 Modbus-TCP server

(The Com'X 200 will work as a pure modbus gateway and will not map any internal variable).

Regards

Jef

See Answer In Context

8 Replies 8
sesa41698_bridg
Lt. Commander Lt. Commander
Lt. Commander

Re: ComX 200 - Modbus gateway support and PME7.2 support

The modbus gateway feature will be included in Com'X 200 version 1.1

This version 1.1 will be available mid March 2014

In this version 1.1, it will not be possible to read the Digital Input neither the Analog Input in the Com'X 200 Modbus-TCP server

(The Com'X 200 will work as a pure modbus gateway and will not map any internal variable).

Regards

Jef

JamesAZZO
Sisko | EcoXpert Master Sisko | EcoXpert Master
Sisko | EcoXpert Master
0 Likes
0
109

Re: ComX 200 - Modbus gateway support and PME7.2 support

Will that feature come later?

sesa56580_bridg
Ensign Ensign
Ensign
0 Likes
3
109

Re: ComX 200 - Modbus gateway support and PME7.2 support

Can you please address the question on regarding COMX 200 support in PME?

nigel_greenwave
Captain | EcoXpert Master Captain | EcoXpert Master
Captain | EcoXpert Master

Re: ComX 200 - Modbus gateway support and PME7.2 support

Hi,

I see a lot of potential with the Comx 200 if the answers "Jan Mikulec" 3 questions were all yes? Is there any road map for this?

Tom_Stevenson
Picard Picard
Picard

Re: ComX 200 - Modbus gateway support and PME7.2 support

Nigel/Jan - as Jef indicates above, the gateway function support is coming, and we are testing this with PME.  For 2 & 3, the file format is the same as the EGX, and would follow the same ETL process used today.

nigel_greenwave
Captain | EcoXpert Master Captain | EcoXpert Master
Captain | EcoXpert Master
0 Likes
0
109

Re: ComX 200 - Modbus gateway support and PME7.2 support

Thanks Tom.

ram_kaushik
Admiral Admiral
Admiral

Re: ComX 200 - Modbus gateway support and PME7.2 support

Wanted to just reiterate the warning to folks so this doesn't get misapplied. This question came up in a commercial training session this week. With the gateway feature in 1.1 currently, PME can only read the connected meters, and  *cannot* read the on-board analog and digital inputs. This could be an issue with WAGES application for example. In the push-to-cloud case, it should be fine.

sesa256952
Schneider Alumni (Retired)
Schneider Alumni (Retired)

Re: ComX 200 - Modbus gateway support and PME7.2 support

when will full support for Comx 200 for PME 7.2. be available.

I need it for a Wages application. In specific gas and water meters.