Gateways and Energy Servers
Schneider Electric support forum to share knowledge about product selection, installation and troubleshooting for EcoStruxure Panel Server, PowerTag, Com'X, Link150…
User | Count |
---|---|
82 | |
46 | |
29 | |
28 |
Link copied. Please paste this link to share this article on your social media post.
Posted: 2015-02-26 05:37 AM
Link copied. Please paste this link to share this article on your social media post.
Nice document !
Please find herebellow some comments to update this doc :
1) Can the Com’X be used as a gateway to connect with PME or PSE
With the latest release of firmware (1.3.5), yes. , the onboard inputs are also available
NOTE : For security reason this feature is disabled by default, and must be configured in the "Initial Settings / Modbus serial", (read the design guide for more information)
4) What about exporting to Energy Operation for a hosted solution ?
Com'X 200 has been designed for exporting data to a hosted solution
All the interfaces can be used (Ethernet, Wi-Fi, GPRS)
7) Can I daisy chain ComX’s and use one as a wireless access point?
Yes, using the "modbus gateway" feature of the 2nd Com'X
😎 When the firmware is ready, will using it in one mode (GPRS for example) disable it in other modes?
The "modbus gateway" feature can be used by a local PME, PSE or scada, while the com'X publishes data to a hosted platform
Warning A) In version 1.3.5, Wifi can be used for configuration, data acquisition and data publication
Regards
Jef
Link copied. Please paste this link to share this article on your social media post.
Hi Jef - thanks for the nice updates but to be clear, I don't want to be the "owner" of this document to update and maintain it. I only posted it an example I had started it last year. I can certainly help contribute to it, but I would like this document to be produced by the Product team.
Link copied. Please paste this link to share this article on your social media post.
Hi guys,
Do you add PM5560 in the last release ?
Can I use STB ?
Regards
Link copied. Please paste this link to share this article on your social media post.
I just saw for PM5560 it was added from version 1.1...
Link copied. Please paste this link to share this article on your social media post.
Yes. As a reminder, here is a link to the latest User Guide for version 1.4.6
https://powersolutionscommunity.schneider-electric.com/docs/DOC-3630
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.