Gateways and Energy Servers
Schneider Electric support forum to share knowledge about product selection, installation and troubleshooting for EcoStruxure Panel Server, PowerTag, Com'X, Link150…
User | Count |
---|---|
82 | |
46 | |
29 | |
28 |
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Hello Moshe,
I am not an expert on SEPAM, but the Com'X 510 does support SEPAM Series 40 and 80 as of Firmware Version 1.1 (release is expected within the week).
I hope this helps.
James
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
From my knowledge of developing the Sepam device driver for PME there typically are few differences within a given family of Sepam devices - ie. very minor differences between a Sepam T42 and a S40 for instance.
Long as the COM'X supports one or more devices in the Sepam 4x family then the Sepam T42 should work even if the T42 is not on the formally supported list, just pick another Sepam 40 from the list with perference to another in the T4x list if possible.
Also: The Sepam 60 family is effectively a cut down variant of the Sepam 80. Since the 60 is relatively new to the market it may not be listed in the COM'X support list. In this case you could try using the Sepam 80 instead and it probably will work in the majority of cases (from what I could tell the 60 just reduced the number of protection units from the 80 and added two new specialized protection unit types).
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.