Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

Com'X510 over a fibre network

Gateways and Energy Servers

Schneider Electric support forum to share knowledge about product selection, installation and troubleshooting for EcoStruxure Panel Server, PowerTag, Com'X, Link150…
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
  • EcoStruxure Power & Grid
  • Gateways and Energy Servers
  • Com'X510 over a fibre network
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Romain_Polette
Kirk Romain_Polette Kirk
117
Guillaume_Evrard
Captain Guillaume_Evrard Captain
59
Randi_Dolan
Commander Randi_Dolan Commander
46
View All

Recommended Forums

  • Metering & Power Quality

  • SmartConnector Forum

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Gateways and Energy Servers
Start a Topic
solutions_iems-
Lt. Commander solutions_iems-
Lt. Commander

Posted: ‎2019-08-23 05:16 AM . Last Modified: ‎2019-08-23 05:19 AM

0 Likes
2
1066
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
‎2019-08-23 05:16 AM

Com'X510 over a fibre network

I have an installation whereby a fibre link via media converters has been installed to allow 2 no. Com'X510 energy servers to communicate with each other over a distance of 250m.

 

One Com'X510 is the master and communicates with the clients network (static IP 10.254.1.100 on Port 1) and two Com'X510 slaves (static IP10.25.1.1 on Port 2).

 

Slave 1 has a static IP of 10.25.1.2 and slave 2 has a static IP of 10.25.1.3 (both connected on Port 2).

 

The master, slave 2 and the fibre link to slave 1 are all connected to a Netgear 5-port switch.

 

The master can communicate with slave 2 but cannot communicate with slave 1.

 

When connecting my laptop to the 5-port switch, this too cannot communicate with slave 1.

 

However, if I go to the other end of the fibre link and connect my laptop, I can ping and browse the master and slave 2.

 

I have also tried slave 2 and an EGX300 in place of slave 1 but neither of these can communicate withe the Master or my laptop PC.

 

Is this a Com'X configuration issue or more likely a fibre link/media converter issue?

 

Any comments will be appreciated.

Reply
  • All forum topics
  • Previous Topic
  • Next Topic
Replies 2
Randi_Dolan
Commander Randi_Dolan Commander
Commander

Posted: ‎2019-08-23 05:43 AM . Last Modified: ‎2019-08-23 08:25 AM

0 Likes
1
1061
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
‎2019-08-23 05:43 AM

Hi,

 

To me, this sounds like an issue with the fiber link/media converter.

 

Regards,

Randi

 

Update:

 

But, after discussing with a co-worker, he believes that the issue cannot be in the converter.  So, to help clarify the situation for us, would you draw a picture of the configuration (I've drawn it from your description but would like to confirm) and attach it to this thread?

 

Thanks,

Randi

Reply
Hal_Etheridge
Janeway Hal_Etheridge Janeway
Janeway

Posted: ‎2019-08-23 11:15 AM

1 Like
0
1055
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
‎2019-08-23 11:15 AM

One way to confirm if it is the media converter or not is to run a temporary twisted pair cable between the COMx devices.  Technically the length between the devices is over the ethernet segment limit but in practice this should work fine for short periods.  Alternatively just bring one of the COMx devices closer to the other for the connectivity test.
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.