Gateways and Energy Servers
Schneider Electric support forum to share knowledge about product selection, installation and troubleshooting for EcoStruxure Panel Server, PowerTag, Com'X, Link150…
User | Count |
---|---|
82 | |
46 | |
29 | |
28 |
Link copied. Please paste this link to share this article on your social media post.
Hello
with com'x200 (firmware 1.1.14) I'm trying to create a custom modbus device. I read and log correctly the measurement (current, voltage, energy, etc.) but I need to log also some digital information.
I create the items as booleans, like this
and I can see them in my device:
But when I export all the hierarchy in EO, these meters are not created, and so its impossible to use these data.
Is that a bug? In the future will be implemented also the option to export these booleans data?
Thanks
Sabrina
Posted: 2014-07-24 09:08 AM
Link copied. Please paste this link to share this article on your social media post.
Hello Sabrina
I have also seen your bug in version 1.1.15 (internal release),
It is now fixed in version 1.1.20 (customer release).
This release has been released today and should be available in gthe comming days on "Shopping-kiosk"
Link copied. Please paste this link to share this article on your social media post.
Hi Sabrina,
I have only see the com x200 in a demo currently and haven had a full hands on play.
One thing I note from your screen shot is the starting register looked at for your booleans (256) is the same as the function line above for numerical variables.
Could that be the issue?
Darren
Link copied. Please paste this link to share this article on your social media post.
Hi Darren
thank you for the answer, but unfortunately this isnt the reason of the issue.
I tried also creating a device with only booleans, and the meters and the data are still not created and exported.
Sabrina
Link copied. Please paste this link to share this article on your social media post.
Hello Sabrina.
Have you submitted a technical support request? If not, I would suggest logging a ticket with them to help resolve this issue.
********
Do you need technical support for the Com'X 200? Just a notice that you can also log support tickets directly via email at global-ems-solutions-support@schneider-electric.com.
Thanks!
James Jeanette | Lazaro Cespedes Miranda
Link copied. Please paste this link to share this article on your social media post.
The support answered me today that it will be solved in the next release of the firmware.
Thanks
Sabrina
Posted: 2014-07-24 09:08 AM
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Hello Sabrina...Com'X 200 Version 1.1.20 is now available on the Shopping Kiosk, or here on the SEC : https://powersolutionscommunity.schneider-electric.com/docs/DOC-2746
Link copied. Please paste this link to share this article on your social media post.
Hi Jef,
I had a question today regarding the logging interval of the Comx200 device when it is set to CSV export: what is the fastest interval the comx200 can log?
Can it do 10 seconds?
I know the online platforms only support > 5 minutes, but this is for offline logging.
Posted: 2015-03-16 04:41 AM
Link copied. Please paste this link to share this article on your social media post.
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.