Ask our Experts
Didn't find what you are looking for? Ask our experts!
Schneider Electric support forum to share knowledge about product selection, installation and troubleshooting for EcoStruxure Panel Server, PowerTag, Com'X, Link150…
Search in
| User | Count |
|---|---|
| 116 | |
| 58 | |
| 46 | |
| 32 |
Posted: 2017-05-16 04:59 PM
Link copied. Please paste this link to share this article on your social media post.
Hello!!
Can anyone explain why, when one configures a static ip address to com port 1 on a Com'x, the config asks for a DNS address? It doesn't really make much sense.
Thanks!
Posted: 2017-05-23 08:34 AM
Link copied. Please paste this link to share this article on your social media post.
Colton Peltier one has to enter the static IP adress of port 1 into 'Primary DNS server' for a static config on port 1.
Firstly, I tried entering the DF gateway address but couldn't connect, no ping back nada, ended up having to do a hard reset and start again.
On another note - I am accessing the ComX via port 1, I'm trying to change port 2 to a static address but it keeps changing back to 'DHCP server'. Any ideas? BTW - the pic I took was after I changed port 2 address/config, as you can see it says dhcp...
Thanks!
Posted: 2017-05-22 06:26 AM
Link copied. Please paste this link to share this article on your social media post.
Hi Brahm,
The DNS server address is used by the ComX to resolve IP addresses from hostnames. For example, many customers may have internal hostnames (within their network) they would like to publish data to. In order to resolve the IP address of the hostname, the ComX needs to know which DNS server to contact.
Best Regards,
Colton
Posted: 2017-05-22 07:22 AM
Link copied. Please paste this link to share this article on your social media post.
Hi Colton,
Thank you for your reply. I think perhaps you misunderstood the question - or - I did not phrase it properly...?
A Com'X is installed on a LAN and has been assigned a static IP address, default gateway and subnet mask. There are no other 'hostnames' on the network as the whole network has been set up for static routing, with port forwarding and NAT handled in the network switches. In this scenario, a DNS is not neccessary as there is no need to resolve a hostnme.
The question really then, I guess, is, what address does one put in the "Primary DNS server" address field if there is no DNS?
Thanks!
Posted: 2017-05-23 06:58 AM
Link copied. Please paste this link to share this article on your social media post.
Hi Brahm,
Good point about it being a required field, with the possibility of it not being needed. The safest bet to enter here if it is not needed is the static IP of the ComX itself, or the configured gateway.
Best Regards!
Posted: 2017-05-23 07:52 AM
Link copied. Please paste this link to share this article on your social media post.
Ok great it's not just me then haha!
Perhaps something that can be rectified in the next firmware release? Less cause for confusion and/or config errors!
Thanks.
Posted: 2017-05-23 08:34 AM
Link copied. Please paste this link to share this article on your social media post.
Colton Peltier one has to enter the static IP adress of port 1 into 'Primary DNS server' for a static config on port 1.
Firstly, I tried entering the DF gateway address but couldn't connect, no ping back nada, ended up having to do a hard reset and start again.
On another note - I am accessing the ComX via port 1, I'm trying to change port 2 to a static address but it keeps changing back to 'DHCP server'. Any ideas? BTW - the pic I took was after I changed port 2 address/config, as you can see it says dhcp...
Thanks!
Posted: 2017-05-23 09:43 AM
Link copied. Please paste this link to share this article on your social media post.
Hi Brahm,
I can't see any screenshots you've attached can you please re-upload? Are you trying to configure both ports to be static IP addresses?
Best Regards,
Colton
Posted: 2017-05-25 08:49 AM
Link copied. Please paste this link to share this article on your social media post.

Apologies! I obviously forgot to attach it!
You’ve reached the end of your document
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.