Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84722members
354123posts

Best way to convert Serial Modbus VarLogic to IEC61850

Gateways and Energy Servers

Get expert answers to your questions regarding Schneider Electric Gateways & Energy Servers, from product selection to implementation and troubleshooting. Collaborate with a global community of experts and peers, get support and share your experiences by subscribing to the Schneider Electric Community Gateways and Energy Servers forum today.

sesa97267_bridg
Lieutenant JG Lieutenant JG
Lieutenant JG
0 Likes
3
122

Best way to convert Serial Modbus VarLogic to IEC61850

Hi,

we have a request to provide data from a Serial Modbus VarLogic in IEC61850 format.

Would you rather advise to use G3200? Did anyone already build the dedicated CID file?

Would you alternately recommend using an IEC 61850 capable meter (PM8000 or ION7650) to perform this?

Best regards

Tags (2)
3 Replies 3
Adrian_Dicea
Janeway Janeway
Janeway
0 Likes
2
87

Re: Best way to convert Serial Modbus VarLogic to IEC61850

Hi Jean-Christophe,

This would fit into Gateways & Energy Servers that's why maybe nobody answered it.

Maybe G3200 would be good, but which Varlogic model, how many registers, what are the IEC61850 conversion requirements?

Not sure if anyone has built a CID file already, I didn't, but I am willing to help you.

Would you alternately recommend using an IEC 61850 capable meter (PM8000 or ION7650) to perform this? It's a very expensive approach vs G3200. Perhaps even after counting the engineering time.

Regards,

Adrian

vijith_alnisfgr
Cadet
0 Likes
1
87

Re: Best way to convert Serial Modbus VarLogic to IEC61850

I have a similar requirement where PM2120 modbus data needs to be converted to IEC61850.Basic electrical parameters like voltage,current,power and energy values are required in IEC61850 format.

Can I use G3200?

Adrian_Dicea
Janeway Janeway
Janeway
0 Likes
0
86

Re: Best way to convert Serial Modbus VarLogic to IEC61850

Yes, Ed.1 only.