Are there any plans to include EM4800 series meters into EGX300?

Gateways and Energy Servers

Schneider Electric support forum to share knowledge about product selection, installation and troubleshooting for EcoStruxure Panel Server, PowerTag, Com'X, Link150…
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
  • EcoStruxure Power & Grid
  • Gateways and Energy Servers
  • Are there any plans to include EM4800 series meters into EGX300?
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Romain_Polette
Kirk Romain_Polette Kirk
116
Guillaume_Evrard
Captain Guillaume_Evrard Captain
58
Randi_Dolan
Commander Randi_Dolan Commander
46
View All

Recommended Forums

  • Metering & Power Quality

  • SmartConnector Forum

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Solved Go to Solution
Back to Gateways and Energy Servers
Start a Topic
Solved
Digital_Hastak
Lieutenant JG Digital_Hastak Lieutenant JG
Lieutenant JG

Posted: ‎2013-04-30 06:46 PM

0 Likes
8
1687
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
‎2013-04-30 06:46 PM

Are there any plans to include EM4800 series meters into EGX300?

Also do we have any tested Custom Device files that would work with EM4800? I have tried creating custom device, but have been getting intermitted comms issue. I will try them again, and can share here.

Tags (1)
  • Tags:
  • egx300
Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
JamesJeanette
Commander JamesJeanette Commander
Commander

Posted: ‎2013-06-19 02:21 PM

3 Likes
4
1577
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
‎2013-06-19 02:21 PM

Just an update...We are planning to release the EM4800 in our next release!  Look for it in just a few weeks.

James

See Answer In Context

Reply
Replies 8
sesa64390_bridg
Lt. Commander sesa64390_bridg Lt. Commander
Lt. Commander

Posted: ‎2013-05-01 10:06 AM

0 Likes
0
1577
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
‎2013-05-01 10:06 AM

Hi Hastak,

You can program the EM4800 to log the values onboard and then the EM4800 can FTP those data files to where ever you need them (the files are a .TR3 but you can open and read them in Notepad).

If you need to import that data into a software platform like Energy Operation (so that you can display the data) then you could use the to convert those files into a consumable format for the software platform (EEM, EO, etc).

Of course this doesn't help you if you want to display the EM4800 values on the EGX300 itself, but it does give you alternatives if you are having issues integrating EM4800 on EGX300.

Colin

Reply
Digital_Hastak
Lieutenant JG Digital_Hastak Lieutenant JG
Lieutenant JG

Posted: ‎2013-05-01 03:21 PM

0 Likes
0
1577
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
‎2013-05-01 03:21 PM

Good day Colin,

I have used the onboard logging and FTP function and am aware of EM4800's functions. However, we have a growing demand from various customer projects where they want to be able to map EM4800 data via EGX.

EM4800 is a very good meter in terms of its size/form factor and features, but it has its own software and also its web server/page is not very user-friendly and helpful. Hence we get regular queries from customers regarding this.

I will try and create templates for custom device locally and see if it works. If successful will share it with everyone.

Hastak

Reply
JamesJeanette
Commander JamesJeanette Commander
Commander

Posted: ‎2013-05-16 07:22 AM

1 Like
0
1577
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
‎2013-05-16 07:22 AM

Hello Hastak.

We received a request from the Power Monitoring Offer Manager this morning to have the EM4800 officially supported in the EGX300.  We will be working closely with his team to define what is needed to add and support the device.

Thanks,

James Jeanette 

Reply
JamesJeanette
Commander JamesJeanette Commander
Commander

Posted: ‎2013-06-19 02:21 PM

3 Likes
4
1578
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
‎2013-06-19 02:21 PM

Just an update...We are planning to release the EM4800 in our next release!  Look for it in just a few weeks.

James

Reply
sesa101714_brid
Ensign sesa101714_brid Ensign
Ensign

Posted: ‎2013-06-28 06:05 AM

0 Likes
3
1577
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
‎2013-06-28 06:05 AM

Hi James,

Is trending going to be supported for the EM4800?

Thanks,

Amelia

Reply
JamesJeanette
Commander JamesJeanette Commander
Commander

Posted: ‎2013-06-28 09:00 AM

0 Likes
2
1577
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
‎2013-06-28 09:00 AM

No, sorry trending will not be supported as the EM4800 acts like a BCM or BCPM.  The EGX300 doesn't do trending when you have channels, or circuits.

Thanks

Reply
sesa285874
sesa285874 Schneider Alumni (Retired)
Schneider Alumni (Retired)

Posted: ‎2014-09-18 09:34 AM

0 Likes
1
1577
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
‎2014-09-18 09:34 AM

Hi James,

I was trying to read an EM4800 into an EGX300 by using the default device type which is included in the new firmware. It turned out that the EGX started reading and suddenly went into time-out. By reading in MODSCAN, I figured out that the meter can only handle 16registers at the same time so I created a new device type by using the web-based tool included in the EGX300 since you cannot edit a default device type. My question is if there is a new release for the EGX-300 that can handle this or maybe I can edit the defualt device type somehow as the client do not want to lose the other capabilities that default meters have (layout, trending, etc).

Any help will be much appreciated.

Regards

Reply
JamesJeanette
Commander JamesJeanette Commander
Commander

Posted: ‎2014-09-18 09:54 AM

0 Likes
0
1577
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
‎2014-09-18 09:54 AM

Hi Juan,

Can you tell me which Firmware Version and Disk Update Version you are using on the EGX300?

As a reminder..you can log into your EGX300, and look to the bottom left for your version:

4704

Copying for context.
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.