Add multiple I/Os to Can2Go SSL using Advantys OTB Modicon
Gateways and Energy Servers
Schneider Electric support forum to share knowledge about product selection, installation and troubleshooting for EcoStruxure Panel Server, PowerTag, Com'X, Link150…
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
You have entered an invalid email address. Please re-enter the email address.
This co-worker has already been invited to the Exchange portal. Please invite another co-worker.
Please enter email address
Send InviteCancel
Invitation Sent
Your invitation was sent.Thanks for sharing Exchange with your co-worker.
Link copied. Please paste this link to share this article on your social media post.
2014-12-0307:02 PM
Add multiple I/Os to Can2Go SSL using Advantys OTB Modicon
Overview
Since MPM has limited build-in IOs, and the TE2 is also limited in terms of I/Os, we will explore the possibilities of using Advantys OTB (Optimized Terminal Block) as the extension IO Module for Can2go/SSL controllers.
The Advantys supports several communication protocols (Modbus RTU, Modbus TCP and CANOpen ) with different Network Modules, however in this article, we will focus on Modbus TCP integration and we'll look at others later.
Devices Used
SSL UN Controller
OTB 1E0DM9LP
24 V DC Power supply
Key Setup Steps
Setup the IP address of OTB (using DHCP)
* for fix IP assignment, please refer to <<Advantys OTB User Manual.pdf>> for more details
Write a Lua script to read the DIs of OTB and control the DOs