Gateways and Energy Servers
Schneider Electric support forum to share knowledge about product selection, installation and troubleshooting for EcoStruxure Panel Server, PowerTag, Com'X, Link150…
User | Count |
---|---|
82 | |
46 | |
29 | |
28 |
Link copied. Please paste this link to share this article on your social media post.
1. With a SIM10M connected to the EGX is it possible to rename the inputs? Currently I read DI1 and DI2. I would like to rename this to gas and wtaer. Especially in the dashboards in the EGX.
2. We connected an PM750 to the EGX300 and use the DI to count gas pulses. The countervalue can be read in ION6 but I can not see the value in the EGX300 history or dashboards.
3. We have experimented with the custom pages in the EGX300. Is it possible to access the historical data? I know the dashbiards are able to display historical data but are custom pages also allowed?
4. In the custom webpages we want to use icons (logo's) to navigate. Are any icons from Schneider availiable? (like the ones used in the Energy Server Com X 200 video ) (gas, water , temperature etc)
Hopefully someone can answer these questions.
Regards Jos Gräfe (and Lieven van Belzen) Beenen Netherlands.
Link copied. Please paste this link to share this article on your social media post.
Hi Jos!
1) Do a custom device type and do a Custom Unit of Measure.
2) Same answer. Many meter's implementation don't have the extra DI input registers. I know, it used to be the case for the PM3255 for example. If you create your customer device type, you should be just fine.
3-4) Not sure, sorry.
Link copied. Please paste this link to share this article on your social media post.
Hello Jos,
3) Unfortunately, with the current directory structure, the data log files are not available via HTTP. This feature could be added. Please consult James Jeanette to inquire about adding this feature.
4) James Jeanette can also help you with locating images available for use.
Randi
Link copied. Please paste this link to share this article on your social media post.
Hi Jos,
3) We are very limited on what we can add to the EGX300, but if there is a strong business case for adding this, please let me know via email so that I can add it to the list to be assessed. You can reach me by email at james.jeanette@schneider-electric.com.
4) There are Schneider Electric logos and branding information available such as you have seen in the Com'X 200 video; however I do not know what is available to share outside of Schneider.
Maybe start here:
Visit http://brandbook.schneider-electric.com
Thanks,
James
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.